PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_SET_BCAST_MCAST_LIMIT command.
Data Fields | |
bool | rateLimitAtTxPort |
uint32_t | numPorts |
CpswAle_PortBcastMcastRateLimitParams | portPrms [CPSW_ALE_NUM_PORTS] |
bool CpswAle_SetBcastMcastRateLimitInArgs::rateLimitAtTxPort |
Rate limit to be done at transmit or receive port
uint32_t CpswAle_SetBcastMcastRateLimitInArgs::numPorts |
Number of port for which broadcast/multicast rate limiting config to be applied
CpswAle_PortBcastMcastRateLimitParams CpswAle_SetBcastMcastRateLimitInArgs::portPrms[CPSW_ALE_NUM_PORTS] |
Per port broadcast/multicast rate limit params