PDK API Guide for J721E
|
Port specific VLAN security configuration.
Data Fields | |
bool | vidIngressCheck |
bool | dropUntagged |
bool | dropDualVlan |
bool | dropDoubleVlan |
bool CpswAle_PortVlanSecurityCfg::vidIngressCheck |
VLAN ID Ingress Check
bool CpswAle_PortVlanSecurityCfg::dropUntagged |
Drop untagged packets
bool CpswAle_PortVlanSecurityCfg::dropDualVlan |
Drop Dual VLAN - When set will cause any received packet with dual VLAN stag followed by ctag to be dropped
bool CpswAle_PortVlanSecurityCfg::dropDoubleVlan |
Drop Double VLAN - When set cause any received packet with double VLANs to be dropped. That is if there are two ctag or two stag fields in the packet it will be dropped