PDK API Guide for J721E
pmic_irq_lp8764x.h File Reference
PMIC Driver
»
PMIC Interrupt Driver API.
Introduction
LP8764x Hera PMIC IRQ Driver API/interface file.
Go to the source code of this file.
Macros
PMIC IRQ Interrupt values for LP8764x HERA PMIC Device.
#define
PMIC_LP8764X_WD_RST_INT
(0U)
#define
PMIC_LP8764X_WD_FAIL_INT
(1U)
#define
PMIC_LP8764X_WD_LONGWIN_TIMEOUT_INT
(2U)
#define
PMIC_LP8764X_ESM_MCU_RST_INT
(3U)
#define
PMIC_LP8764X_ESM_MCU_FAIL_INT
(4U)
#define
PMIC_LP8764X_ESM_MCU_PIN_INT
(5U)
#define
PMIC_LP8764X_NRSTOUT_SOC_READBACK_INT
(6U)
#define
PMIC_LP8764X_EN_DRV_READBACK_INT
(7U)
#define
PMIC_LP8764X_I2C2_ADR_ERR_INT
(8U)
#define
PMIC_LP8764X_I2C2_CRC_ERR_INT
(9U)
#define
PMIC_LP8764X_COMM_ADR_ERR_INT
(10U)
#define
PMIC_LP8764X_COMM_CRC_ERR_INT
(11U)
#define
PMIC_LP8764X_COMM_FRM_ERR_INT
(12U)
#define
PMIC_LP8764X_SOC_PWR_ERR_INT
(13U)
#define
PMIC_LP8764X_MCU_PWR_ERR_INT
(14U)
#define
PMIC_LP8764X_ORD_SHUTDOWN_INT
(15U)
#define
PMIC_LP8764X_IMM_SHUTOWN_INT
(16U)
#define
PMIC_LP8764X_PFSM_ERR_INT
(17U)
#define
PMIC_LP8764X_VCCA_OVP_INT
(18U)
#define
PMIC_LP8764X_TSD_IMM_INT
(19U)
#define
PMIC_LP8764X_NRSTOUT_READBACK_INT
(20U)
#define
PMIC_LP8764X_NINT_READBACK_INT
(21U)
#define
PMIC_LP8764X_SPMI_ERR_INT
(22U)
#define
PMIC_LP8764X_RECOV_CNT_INT
(23U)
#define
PMIC_LP8764X_REG_CRC_ERR_INT
(24U)
#define
PMIC_LP8764X_BIST_FAIL_INT
(25U)
#define
PMIC_LP8764X_TSD_ORD_INT
(26U)
#define
PMIC_LP8764X_TWARN_INT
(27U)
#define
PMIC_LP8764X_EXT_CLK_INT
(28U)
#define
PMIC_LP8764X_BIST_PASS_INT
(29U)
#define
PMIC_LP8764X_FSD_INT
(30U)
#define
PMIC_LP8764X_ENABLE_INT
(31U)
#define
PMIC_LP8764X_GPIO8_INT
(32U)
#define
PMIC_LP8764X_GPIO7_INT
(33U)
#define
PMIC_LP8764X_GPIO6_INT
(34U)
#define
PMIC_LP8764X_GPIO5_INT
(35U)
#define
PMIC_LP8764X_GPIO4_INT
(36U)
#define
PMIC_LP8764X_GPIO3_INT
(37U)
#define
PMIC_LP8764X_GPIO2_INT
(38U)
#define
PMIC_LP8764X_GPIO1_INT
(39U)
#define
PMIC_LP8764X_GPIO10_INT
(40U)
#define
PMIC_LP8764X_GPIO9_INT
(41U)
#define
PMIC_LP8764X_VMON2_RV_INT
(42U)
#define
PMIC_LP8764X_VMON2_UV_INT
(43U)
#define
PMIC_LP8764X_VMON2_OV_INT
(44U)
#define
PMIC_LP8764X_VMON1_RV_INT
(45U)
#define
PMIC_LP8764X_VMON1_UV_INT
(46U)
#define
PMIC_LP8764X_VMON1_OV_INT
(47U)
#define
PMIC_LP8764X_VCCA_UV_INT
(48U)
#define
PMIC_LP8764X_VCCA_OV_INT
(49U)
#define
PMIC_LP8764X_BUCK4_ILIM_INT
(50U)
#define
PMIC_LP8764X_BUCK4_SC_INT
(51U)
#define
PMIC_LP8764X_BUCK4_UV_INT
(52U)
#define
PMIC_LP8764X_BUCK4_OV_INT
(53U)
#define
PMIC_LP8764X_BUCK3_ILIM_INT
(54U)
#define
PMIC_LP8764X_BUCK3_SC_INT
(55U)
#define
PMIC_LP8764X_BUCK3_UV_INT
(56U)
#define
PMIC_LP8764X_BUCK3_OV_INT
(57U)
#define
PMIC_LP8764X_BUCK2_ILIM_INT
(58U)
#define
PMIC_LP8764X_BUCK2_SC_INT
(59U)
#define
PMIC_LP8764X_BUCK2_UV_INT
(60U)
#define
PMIC_LP8764X_BUCK2_OV_INT
(61U)
#define
PMIC_LP8764X_BUCK1_ILIM_INT
(62U)
#define
PMIC_LP8764X_BUCK1_SC_INT
(63U)
#define
PMIC_LP8764X_BUCK1_UV_INT
(64U)
#define
PMIC_LP8764X_BUCK1_OV_INT
(65U)
#define
PMIC_LP8764X_SOFT_REBOOT_INT
(66U)
#define
PMIC_LP8764X_IRQ_MAX_NUM_PG_1_0
(66U)
#define
PMIC_LP8764X_IRQ_MAX_NUM_PG_2_0
(67U)
PMIC GPIO Interrupt Mask values for tps6594x.
#define
PMIC_LP8764X_IRQ_GPIO_1_INT_MASK_NUM
(0U)
#define
PMIC_LP8764X_IRQ_GPIO_2_INT_MASK_NUM
(1U)
#define
PMIC_LP8764X_IRQ_GPIO_3_INT_MASK_NUM
(2U)
#define
PMIC_LP8764X_IRQ_GPIO_4_INT_MASK_NUM
(3U)
#define
PMIC_LP8764X_IRQ_GPIO_5_INT_MASK_NUM
(4U)
#define
PMIC_LP8764X_IRQ_GPIO_6_INT_MASK_NUM
(5U)
#define
PMIC_LP8764X_IRQ_GPIO_7_INT_MASK_NUM
(6U)
#define
PMIC_LP8764X_IRQ_GPIO_8_INT_MASK_NUM
(7U)
#define
PMIC_LP8764X_IRQ_GPIO_9_INT_MASK_NUM
(8U)
#define
PMIC_LP8764X_IRQ_GPIO_10_INT_MASK_NUM
(9U)
packages
ti
drv
pmic
include
cfg
lp8764x
pmic_irq_lp8764x.h
Generated by
1.8.15