![]() |
PDK API Guide for J721E
|
Interface file for SDE M2M FVID2 driver
Files | |
file | vhwa_m2mSde.h |
Defines the structures / control operations that could be used to configure / control SDE M2M driver. | |
Data Structures | |
struct | Vhwa_M2mSdePrms |
Connfiguration parameters of SDE. More... | |
struct | Vhwa_M2mSdeCreateArgs |
Parameters required to create a new handle. More... | |
struct | Vhwa_M2mSdeInitParams |
Initialization Parameters for SDE M2M Driver. More... | |
struct | Vhwa_M2mSdeSl2AllocPrms |
Init Parameters required to allocate SDE driver. More... | |
Functions | |
static void | Vhwa_M2mSdeInitParamsInit (Vhwa_M2mSdeInitParams *sdeInitPrms) |
Vhwa_M2mSdeInitParams structure init function. More... | |
static void | Vhwa_M2mSdePrmsInit (Vhwa_M2mSdePrms *sdePrms) |
Function to initialize the SDE configuration parameters to default. More... | |
static void | Vhwa_M2mSdeCreateArgsInit (Vhwa_M2mSdeCreateArgs *createArgs) |
Function to initialize the SDE create argument parameters to default. More... | |
int32_t | Vhwa_m2mSdeInit (Vhwa_M2mSdeInitParams *pInitPrms) |
SDE initialization function. This function initializes the SDE hardware and drivers. This function should be called before calling any driver APIs and only once. More... | |
void | Vhwa_m2mSdeDeInit (void) |
SDE de-initialization function. This function un-initializes the SDE hardware and drivers. This function should be called during system shutdown if Vhwa_m2mSdeDeInit() was called by the application. More... | |
int32_t | Vhwa_m2mSdeAllocSl2 (const Vhwa_M2mSdeSl2AllocPrms *sl2allocPrms) |
Function to allocate Sl2 memory for input and output buffers. Both DOF and SDE SL2 memory should be freed before reallocating. More... | |
int32_t | Vhwa_m2mSdeFreeSl2 (void) |
Function to free allocated SL2. More... | |
static void | Vhwa_M2mSdeSl2AllocPrmsInit (Vhwa_M2mSdeSl2AllocPrms *prms) |
Macros | |
#define | VHWA_M2M_SDE_MAX_IN_BUFFER (2U) |
#define | VHWA_M2M_SDE_MAX_OUT_BUFFER (1U) |
#define | VHWA_M2M_SDE_MAX_BUFFER |
#define | VHWA_M2M_SDE_DRV_INST_ID (0U) |
#define | VHWA_M2M_SDE_MAX_HANDLES (4u) |
Max Number of handles supported by SDE M2M Driver. More... | |
VHWA SDE IOCTL macros | |
#define | VHWA_M2M_IOCTL_SDE_SET_PARAMS (VHWA_IOCTL_SDE_IOCTL_BASE) |
IOCTL for setting SDE configuration. More... | |
#define | VHWA_M2M_IOCTL_SDE_SET_HTS_LIMIT (VHWA_M2M_IOCTL_SDE_SET_PARAMS + 1u) |
IOCTL for setting bandwidth limiter. More... | |
#define | VHWA_M2M_IOCTL_SDE_GET_PERFORMANCE (VHWA_M2M_IOCTL_SDE_SET_HTS_LIMIT + 1u) |
IOCTL for getting IP performance. More... | |
#define | VHWA_M2M_IOCTL_SDE_GET_PSA_SIGN (VHWA_M2M_IOCTL_SDE_GET_PERFORMANCE + 1u) |
IOCTL for getting the PSA signature. More... | |
#define | VHWA_M2M_IOCTL_SDE_GET_HISTOGRAM (VHWA_M2M_IOCTL_SDE_GET_PSA_SIGN + 1u) |
IOCTL for getting flow vector histogram. More... | |
#define | VHWA_M2M_IOCTL_SDE_REGISTER_ERR_CB (VHWA_M2M_IOCTL_SDE_GET_HISTOGRAM + 1u) |
IOCTL for registering the Error Callback. More... | |
#define | VHWA_M2M_IOCTL_SDE_SYNC_START (VHWA_M2M_IOCTL_SDE_REGISTER_ERR_CB + 1u) |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing. More... | |
VHWA SDE IO buffer indexes | |
#define | SDE_INPUT_REFERENCE_IMG (0U) |
#define | SDE_INPUT_BASE_IMG (1U) |
#define | SDE_OUTPUT (2U) |
#define | SDE_INPUT_FOCO_REF_IMG (3U) |
#define | SDE_INPUT_FOCO_BASE_IMG (4U) |
VHWA SDE Default Init Paramters | |
#define | SDE_DEFAULT_IMG_WIDTH (1280U) |
#define | SDE_DEFAULT_CCSF (FVID2_CCSF_BITS12_UNPACKED16) |
#define | SDE_DEFAULT_DIS_BUFF_DEPTH (2U) |
#define | SDE_DEFAULT_SR (SDE_SR_128) |
#define VHWA_M2M_IOCTL_SDE_SET_PARAMS (VHWA_IOCTL_SDE_IOCTL_BASE) |
IOCTL for setting SDE configuration.
#define VHWA_M2M_IOCTL_SDE_SET_HTS_LIMIT (VHWA_M2M_IOCTL_SDE_SET_PARAMS + 1u) |
IOCTL for setting bandwidth limiter.
#define VHWA_M2M_IOCTL_SDE_GET_PERFORMANCE (VHWA_M2M_IOCTL_SDE_SET_HTS_LIMIT + 1u) |
IOCTL for getting IP performance.
#define VHWA_M2M_IOCTL_SDE_GET_PSA_SIGN (VHWA_M2M_IOCTL_SDE_GET_PERFORMANCE + 1u) |
IOCTL for getting the PSA signature.
#define VHWA_M2M_IOCTL_SDE_GET_HISTOGRAM (VHWA_M2M_IOCTL_SDE_GET_PSA_SIGN + 1u) |
IOCTL for getting flow vector histogram.
#define VHWA_M2M_IOCTL_SDE_REGISTER_ERR_CB (VHWA_M2M_IOCTL_SDE_GET_HISTOGRAM + 1u) |
IOCTL for registering the Error Callback.
#define VHWA_M2M_IOCTL_SDE_SYNC_START (VHWA_M2M_IOCTL_SDE_REGISTER_ERR_CB + 1u) |
IOCTL to sync start each module This IOCTL doesn't configure any register and only enable pipeline to start processing.
#define VHWA_M2M_SDE_MAX_IN_BUFFER (2U) |
Maximim number of inputs SDE buffers
#define VHWA_M2M_SDE_MAX_OUT_BUFFER (1U) |
Maximim number of output SDE buffers
#define VHWA_M2M_SDE_MAX_BUFFER |
Maximim number of total SDE buffers Instance ID for the SDE M2m driver
#define VHWA_M2M_SDE_DRV_INST_ID (0U) |
#define VHWA_M2M_SDE_MAX_HANDLES (4u) |
Max Number of handles supported by SDE M2M Driver.
#define SDE_INPUT_REFERENCE_IMG (0U) |
#define SDE_INPUT_BASE_IMG (1U) |
#define SDE_OUTPUT (2U) |
#define SDE_INPUT_FOCO_REF_IMG (3U) |
#define SDE_INPUT_FOCO_BASE_IMG (4U) |
#define SDE_DEFAULT_IMG_WIDTH (1280U) |
#define SDE_DEFAULT_CCSF (FVID2_CCSF_BITS12_UNPACKED16) |
#define SDE_DEFAULT_DIS_BUFF_DEPTH (2U) |
#define SDE_DEFAULT_SR (SDE_SR_128) |
|
inlinestatic |
Vhwa_M2mSdeInitParams structure init function.
sdeInitPrms | Pointer to Vhwa_M2mSdeInitParams structure. |
|
inlinestatic |
Function to initialize the SDE configuration parameters to default.
sdePrms | Pointer to a Vhwa_M2mSdePrms containing SDE configuration |
|
inlinestatic |
Function to initialize the SDE create argument parameters to default.
createArgs | Pointer to a Vhwa_M2mSdeCreateArgs containing SDE create arguments |
int32_t Vhwa_m2mSdeInit | ( | Vhwa_M2mSdeInitParams * | pInitPrms | ) |
SDE initialization function. This function initializes the SDE hardware and drivers. This function should be called before calling any driver APIs and only once.
pInitPrms | Pointer to a Vhwa_M2mSdeInitParams structure containing the SDE driver initialization parameters |
void Vhwa_m2mSdeDeInit | ( | void | ) |
SDE de-initialization function. This function un-initializes the SDE hardware and drivers. This function should be called during system shutdown if Vhwa_m2mSdeDeInit() was called by the application.
int32_t Vhwa_m2mSdeAllocSl2 | ( | const Vhwa_M2mSdeSl2AllocPrms * | sl2allocPrms | ) |
Function to allocate Sl2 memory for input and output buffers. Both DOF and SDE SL2 memory should be freed before reallocating.
sl2allocPrms | Pointer to a Vhwa_M2mSdeSl2AllocPrms structure containing the SL2 allocation parameters |
int32_t Vhwa_m2mSdeFreeSl2 | ( | void | ) |
Function to free allocated SL2.
|
inlinestatic |