![]() |
PDK API Guide for J721E
|
This Module explains about PMIC FSM driver parameters and APIs usage. PMIC FSM Driver module covers all FSM features APIs. Like, set/get FSM states, enable FSM I2C Triggers, Mask and Unmask NSLEEP Signals and trigger Runtime BIST
Supported PMIC devices for FSM Module:
Files | |
file | pmic_fsm.h |
PMIC Low Level Driver API/interface file for FSM API. | |
Data Structures | |
struct | Pmic_FsmCfg_t |
PMIC FSM configuration structure. Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs. More... | |
Functions | |
int32_t | Pmic_fsmDeviceOffRequestCfg (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t eventType, uint8_t fsmState) |
API to initiate OFF Request FSM transition. More... | |
int32_t | Pmic_fsmDeviceOnRequest (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to initiate ON Request FSM transition. More... | |
int32_t | Pmic_fsmSetMissionState (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pmicState) |
API to Set FSM mission States. More... | |
int32_t | Pmic_fsmSetNsleepSignalMask (Pmic_CoreHandle_t *pPmicCoreHandle, const bool nsleepType, const bool maskEnable) |
API to MASK/UNMASK NSLEEP1B or 2B Signal. More... | |
int32_t | Pmic_fsmGetNsleepSignalMaskStat (Pmic_CoreHandle_t *pPmicCoreHandle, const bool nsleepType, bool *pNsleepStat) |
API to read the status of the NSLEEP1B/2B Signal is masked or not. More... | |
int32_t | Pmic_fsmRequestRuntimeBist (Pmic_CoreHandle_t *pPmicCoreHandle) |
API to initiate Runtime BIST. More... | |
int32_t | Pmic_fsmSetConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, const Pmic_FsmCfg_t fsmCfg) |
API to set PMIC FSM configuration. More... | |
int32_t | Pmic_fsmGetConfiguration (Pmic_CoreHandle_t *pPmicCoreHandle, Pmic_FsmCfg_t *pFsmCfg) |
API to get PMIC FSM configuration. More... | |
int32_t | Pmic_fsmSetPfsmDelay (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t pFsmDelayType, const uint8_t pfsmDelay) |
API to configure PFSM Delay. More... | |
int32_t | Pmic_fsmGetPfsmDelay (Pmic_CoreHandle_t *pPmicCoreHandle, uint8_t pFsmDelayType, uint8_t *pPfsmDelay) |
API to read PFSM Delay. More... | |
int32_t | Pmic_fsmSetNsleepSignalVal (Pmic_CoreHandle_t *pPmicCoreHandle, const bool nsleepType, const uint8_t nsleepVal) |
API to set PMIC Nsleep1B/2B Signal value. More... | |
int32_t | Pmic_fsmGetNsleepSignalVal (Pmic_CoreHandle_t *pPmicCoreHandle, const bool nsleepType, uint8_t *pNsleepVal) |
API to get PMIC Nsleep1B/2B Signal value. More... | |
int32_t | Pmic_fsmRecoverSocPwrErr (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t nsleepVal) |
API to recover from SOC Power Error using Nsleep1B and Nsleep2B signal. More... | |
int32_t | Pmic_fsmEnableI2cTrigger (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t i2cTriggerType, const uint8_t i2cTriggerVal) |
API to initiate FSM I2C trigger for given FSM I2C trigger type. More... | |
int32_t | Pmic_fsmGetI2cTriggerVal (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t i2cTriggerType, uint8_t *pI2cTriggerVal) |
API to get FSM I2C trigger Value for given FSM I2C trigger type. More... | |
int32_t | Pmic_fsmRequestDdrGpioRetentionMode (Pmic_CoreHandle_t *pPmicCoreHandle, const uint8_t retentionMode, const uint8_t i2cTriggerVal) |
API to initiate DDR/GPIO Retention Mode. More... | |
PMIC FSM Off Request Type | |
#define | PMIC_FSM_I2C_TRIGGER0_TYPE (0U) |
#define | PMIC_FSM_ENABLE_PIN_TYPE (1U) |
#define | PMIC_FSM_NPWRON_PIN_TYPE (2U) |
To Select PMIC FSM State | |
#define | PMIC_FSM_STANBY_STATE (0U) |
#define | PMIC_FSM_LP_STANBY_STATE (1U) |
#define | PMIC_FSM_ACTIVE_STATE (2U) |
#define | PMIC_FSM_MCU_ONLY_STATE (3U) |
#define | PMIC_FSM_S2R_STATE (4U) |
PMIC Nsleep Signals | |
#define | PMIC_NSLEEP1_SIGNAL (bool)false |
#define | PMIC_NSLEEP2_SIGNAL (bool)true |
PMIC Nsleep Masking/Unmasking | |
#define | PMIC_NSLEEPX_MASK (1U) |
#define | PMIC_NSLEEPX_UNMASK (0U) |
PMIC Fast BIST Enable/Disable | |
This affects whether or not LBIST can be skipped to save boot up time from LP_STANDBY state. Application need to configure this before the device is turned off (using ENABLE pin or TRIGGER_I2C_0 bit) and enters LP_STANDBY state | |
#define | PMIC_FSM_FAST_BIST_ENABLE (1U) |
Only analog BIST is run at BOOT BIST. More... | |
#define | PMIC_FSM_FAST_BIST_DISABLE (0U) |
Logic and analog BIST is run at BOOT BIST. More... | |
PMIC Nsleep FSM configuration | |
#define | PMIC_NSLEEP1B_FSM_UNMASK (0U) |
#define | PMIC_NSLEEP1B_FSM_MASK (1U) |
#define | PMIC_NSLEEP2B_FSM_UNMASK (0U) |
#define | PMIC_NSLEEP2B_FSM_MASK (1U) |
Select PMIC FSM Startup Destination | |
#define | PMIC_FSM_STARTUPDEST_STANDBY_LPSTANDBY (0U) |
Selects PMIC FSM Startup Destination as STANDBY state or LPSTANDBY state based on LP_STANDBY_SEL. More... | |
#define | PMIC_FSM_STARTUPDEST_MCUONLY (2U) |
Selects PMIC FSM Startup Destination as MCU only state. More... | |
#define | PMIC_FSM_STARTUPDEST_ACTIVE (3U) |
Selects PMIC FSM Startup Destination as Active state. More... | |
PMIC LPSTANDBY State Selection | |
#define | PMIC_FSM_SELECT_LPSTANDBY_STATE (1U) |
#define | PMIC_FSM_SELECT_STANDBY_STATE (0U) |
To Enable/Disable PMIC Buck/LDO regulators ILIM interrupts affect | |
#define | PMIC_FSM_ILIM_INT_FSMCTRL_ENABLE (1U) |
#define | PMIC_FSM_ILIM_INT_FSMCTRL_DISABLE (0U) |
PMIC PFSM Delay Type | |
#define | PMIC_PFSM_DELAY1 (0U) |
#define | PMIC_PFSM_DELAY2 (1U) |
#define | PMIC_PFSM_DELAY3 (2U) |
#define | PMIC_PFSM_DELAY4 (3U) |
PMIC FSM Configuration Structure Param Bits | |
PMIC FSM valid params configuration type for the structure member validParams of Pmic_FsmCfg_t structure | |
#define | PMIC_FSM_CFG_FAST_BIST_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Fast BIST More... | |
#define | PMIC_FSM_CFG_LP_STANDBYSEL_VALID (1U) |
validParams value used to set/get Low Power Standby State Selection More... | |
#define | PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID (2U) |
validParams value used to set/get to Enable/Disable Buck/LDO regulators ILIM interrupts affect FSM triggers More... | |
#define | PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID (3U) |
validParams value used to set/get to Select FSM Startup Destination More... | |
PMIC FSM Configuration valid param bit shift values | |
Application can use below shifted values to set the validParam member defined in Pmic_FsmCfg_t structure | |
#define | PMIC_FSM_CFG_FAST_BIST_EN_VALID_SHIFT (1U << PMIC_FSM_CFG_FAST_BIST_EN_VALID) |
#define | PMIC_FSM_CFG_LP_STANDBYSEL_VALID_SHIFT (1U << PMIC_FSM_CFG_LP_STANDBYSEL_VALID) |
#define | PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID_SHIFT (1U << PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID) |
#define | PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID_SHIFT (1U << PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID) |
PMIC Nsleep 1B/2B signal level | |
#define | PMIC_NSLEEP_LOW (0U) |
#define | PMIC_NSLEEP_HIGH (1U) |
PMIC FSM I2C Trigger Type | |
#define | PMIC_FSM_I2C_TRIGGER0 (0x0U) |
#define | PMIC_FSM_I2C_TRIGGER1 (0x1U) |
Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0. More... | |
#define | PMIC_FSM_I2C_TRIGGER2 (0x2U) |
Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0. More... | |
#define | PMIC_FSM_I2C_TRIGGER3 (0x3U) |
Configuration of PMIC_FSM_I2C_TRIGGER3 is not supported for TPS6594x Leo and LP8764x Hera PMIC. More... | |
#define | PMIC_FSM_I2C_TRIGGER4 (0x4U) |
#define | PMIC_FSM_I2C_TRIGGER5 (0x5U) |
#define | PMIC_FSM_I2C_TRIGGER6 (0x6U) |
#define | PMIC_FSM_I2C_TRIGGER7 (0x7U) |
PMIC FSM I2C Trigger Value | |
#define | PMIC_FSM_I2C_TRIGGER_VAL_0 (0x0U) |
Valid only for I2C4/ I2C5/ I2C6/ I2C7. More... | |
#define | PMIC_FSM_I2C_TRIGGER_VAL_1 (0x1U) |
PMIC FSM Retention Mode | |
#define | PMIC_FSM_DDR_RETENTION_MODE (0x0U) |
#define | PMIC_FSM_GPIO_RETENTION_MODE (0x1U) |
Valid only for J7200 SOC. More... | |
#define PMIC_FSM_I2C_TRIGGER0_TYPE (0U) |
#define PMIC_FSM_ENABLE_PIN_TYPE (1U) |
#define PMIC_FSM_NPWRON_PIN_TYPE (2U) |
#define PMIC_FSM_STANBY_STATE (0U) |
#define PMIC_FSM_LP_STANBY_STATE (1U) |
#define PMIC_FSM_ACTIVE_STATE (2U) |
#define PMIC_FSM_MCU_ONLY_STATE (3U) |
#define PMIC_FSM_S2R_STATE (4U) |
#define PMIC_NSLEEP1_SIGNAL (bool)false |
#define PMIC_NSLEEP2_SIGNAL (bool)true |
#define PMIC_NSLEEPX_MASK (1U) |
#define PMIC_NSLEEPX_UNMASK (0U) |
#define PMIC_FSM_FAST_BIST_ENABLE (1U) |
Only analog BIST is run at BOOT BIST.
#define PMIC_FSM_FAST_BIST_DISABLE (0U) |
Logic and analog BIST is run at BOOT BIST.
#define PMIC_NSLEEP1B_FSM_UNMASK (0U) |
#define PMIC_NSLEEP1B_FSM_MASK (1U) |
#define PMIC_NSLEEP2B_FSM_UNMASK (0U) |
#define PMIC_NSLEEP2B_FSM_MASK (1U) |
#define PMIC_FSM_STARTUPDEST_STANDBY_LPSTANDBY (0U) |
Selects PMIC FSM Startup Destination as STANDBY state or LPSTANDBY state based on LP_STANDBY_SEL.
#define PMIC_FSM_STARTUPDEST_MCUONLY (2U) |
Selects PMIC FSM Startup Destination as MCU only state.
#define PMIC_FSM_STARTUPDEST_ACTIVE (3U) |
Selects PMIC FSM Startup Destination as Active state.
#define PMIC_FSM_SELECT_LPSTANDBY_STATE (1U) |
#define PMIC_FSM_SELECT_STANDBY_STATE (0U) |
#define PMIC_FSM_ILIM_INT_FSMCTRL_ENABLE (1U) |
#define PMIC_FSM_ILIM_INT_FSMCTRL_DISABLE (0U) |
#define PMIC_PFSM_DELAY1 (0U) |
#define PMIC_PFSM_DELAY2 (1U) |
#define PMIC_PFSM_DELAY3 (2U) |
#define PMIC_PFSM_DELAY4 (3U) |
#define PMIC_FSM_CFG_FAST_BIST_EN_VALID (0U) |
validParams value used to set/get to Enable/Disable Fast BIST
#define PMIC_FSM_CFG_LP_STANDBYSEL_VALID (1U) |
validParams value used to set/get Low Power Standby State Selection
#define PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID (2U) |
validParams value used to set/get to Enable/Disable Buck/LDO regulators ILIM interrupts affect FSM triggers
#define PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID (3U) |
validParams value used to set/get to Select FSM Startup Destination
#define PMIC_FSM_CFG_FAST_BIST_EN_VALID_SHIFT (1U << PMIC_FSM_CFG_FAST_BIST_EN_VALID) |
#define PMIC_FSM_CFG_LP_STANDBYSEL_VALID_SHIFT (1U << PMIC_FSM_CFG_LP_STANDBYSEL_VALID) |
#define PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID_SHIFT (1U << PMIC_FSM_CFG_ILIM_INT_FSMCTRL_EN_VALID) |
#define PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID_SHIFT (1U << PMIC_FSM_CFG_FSM_STARTUP_DEST_SEL_VALID) |
#define PMIC_NSLEEP_LOW (0U) |
#define PMIC_NSLEEP_HIGH (1U) |
#define PMIC_FSM_I2C_TRIGGER0 (0x0U) |
#define PMIC_FSM_I2C_TRIGGER1 (0x1U) |
Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0.
#define PMIC_FSM_I2C_TRIGGER2 (0x2U) |
Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0.
#define PMIC_FSM_I2C_TRIGGER3 (0x3U) |
Configuration of PMIC_FSM_I2C_TRIGGER3 is not supported for TPS6594x Leo and LP8764x Hera PMIC.
#define PMIC_FSM_I2C_TRIGGER4 (0x4U) |
#define PMIC_FSM_I2C_TRIGGER5 (0x5U) |
#define PMIC_FSM_I2C_TRIGGER6 (0x6U) |
#define PMIC_FSM_I2C_TRIGGER7 (0x7U) |
#define PMIC_FSM_I2C_TRIGGER_VAL_0 (0x0U) |
Valid only for I2C4/ I2C5/ I2C6/ I2C7.
#define PMIC_FSM_I2C_TRIGGER_VAL_1 (0x1U) |
#define PMIC_FSM_DDR_RETENTION_MODE (0x0U) |
#define PMIC_FSM_GPIO_RETENTION_MODE (0x1U) |
Valid only for J7200 SOC.
int32_t Pmic_fsmDeviceOffRequestCfg | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
uint8_t | eventType, | ||
uint8_t | fsmState | ||
) |
API to initiate OFF Request FSM transition.
Requirement: REQ_TAG(PDK-5851), REQ_TAG(PDK-9159), REQ_TAG(PDK-9329) Design: did_pmic_lpstandby_cfg
This function initiate OFF Request FSM transition from any other mission state to the STANDBY state or the LP_STANDBY state
pPmicCoreHandle | [IN] PMIC Interface Handle. |
eventType | [IN] Event Type used to initiate OFF Request Valid values: Pmic_Fsm_Off_Request_Type |
fsmState | [IN] FSM state. Only Valid for: PMIC_FSM_STANBY_STATE and PMIC_FSM_LP_STANBY_STATE |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmDeviceOnRequest | ( | Pmic_CoreHandle_t * | pPmicCoreHandle | ) |
API to initiate ON Request FSM transition.
Requirement: REQ_TAG(PDK-5837) Design: did_pmic_fsm_cfg_readback
This function setup nSLEEP signal bits with STARTUP_DEST Which is common for all supported PMICs. This API needs to be called at PMIC init before clearing Enable and Start-Up interrupts.
pPmicCoreHandle | [IN] PMIC Interface Handle |
int32_t Pmic_fsmSetMissionState | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | pmicState | ||
) |
API to Set FSM mission States.
Requirement: REQ_TAG(PDK-5837), REQ_TAG(PDK-5851) Design: did_pmic_fsm_cfg_readback, did_pmic_lpstandby_cfg
This function is used for set/change the FSM mission states for PMIC using Nsleep1B and Nsleep2B signals in absence of GPIO pins Note: Application need to unmask Nsleep1B and Nsleep2B signals for FSM state transitions except for Standby/LpStandby State Application need to mask Nsleep1B and Nsleep2B signals for Standby/LpStandby State transition
pPmicCoreHandle | [IN] PMIC Interface Handle |
pmicState | [IN] PMIC FSM mission state Valid values: Pmic_Fsm_Mission_State |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmSetNsleepSignalMask | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const bool | nsleepType, | ||
const bool | maskEnable | ||
) |
API to MASK/UNMASK NSLEEP1B or 2B Signal.
Requirement: REQ_TAG(PDK-5837) Design: did_pmic_fsm_cfg_readback
This function is used for Masking/Unmasking for NSLEEP2B or NSLEEP1B signal.
pPmicCoreHandle | [IN] PMIC Interface Handle |
nsleepType | [IN] NSLEEP signal Valid values: Pmic_Nsleep_Signals |
maskEnable | [IN] Parameter to select masking/unmasking |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmGetNsleepSignalMaskStat | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const bool | nsleepType, | ||
bool * | pNsleepStat | ||
) |
API to read the status of the NSLEEP1B/2B Signal is masked or not.
Requirement: REQ_TAG(PDK-9151) Design: did_pmic_fsm_cfg_readback
This function is used to read the status of the NSLEEP1B/2B Signal is masked or not
pPmicCoreHandle | [IN] PMIC Interface Handle |
nsleepType | [IN] NSLEEP signal Valid values: Pmic_Nsleep_Signals |
pNsleepStat | [OUT] Pointer to store Nsleep Signal is masked or not |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmRequestRuntimeBist | ( | Pmic_CoreHandle_t * | pPmicCoreHandle | ) |
API to initiate Runtime BIST.
Requirement: REQ_TAG(PDK-5849) Design: did_pmic_runtime_bist_cfg
This function initiates a request to exercise runtime BIST on the device Valid only for TPS6594x Leo PMIC PG2.0 and LP8764x Hera PMIC PG2.0
pPmicCoreHandle | [IN] PMIC Interface Handle. |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmSetConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const Pmic_FsmCfg_t | fsmCfg | ||
) |
API to set PMIC FSM configuration.
Requirement: REQ_TAG(PDK-9144), REQ_TAG(PDK-9134), REQ_TAG(PDK-9128) Design: did_pmic_fsm_cfg_readback
This function is used to set the required FSM configuration when corresponding bit field is set.
pPmicCoreHandle | [IN] PMIC Interface Handle. |
fsmCfg | [IN] Set required FSM configuration |
int32_t Pmic_fsmGetConfiguration | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
Pmic_FsmCfg_t * | pFsmCfg | ||
) |
API to get PMIC FSM configuration.
Requirement: REQ_TAG(PDK-9144), REQ_TAG(PDK-9134), REQ_TAG(PDK-9128) Design: did_pmic_fsm_cfg_readback
This function is used to get the FSM configuration when corresponding validParam bit fields are set in Pmic_FsmCfg_t structure
pPmicCoreHandle | [IN] PMIC Interface Handle |
pFsmCfg | [IN/OUT] Pointer to store FSM configuration |
int32_t Pmic_fsmSetPfsmDelay | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | pFsmDelayType, | ||
const uint8_t | pfsmDelay | ||
) |
API to configure PFSM Delay.
Requirement: REQ_TAG(PDK-9136) Design: did_pmic_pfsm_cfg_readback
This function is used to configure PFSM Delay. PFSM Delay will affect the total power up sequence time before the system is released from reset Consider If the PFSM_Delay value is 'x' then Delay will calculated as Delay = x *(50ns * 2^PFSM_DELAY_STEP) Note: In this API, the default delay Type is assumed as PMIC_PFSM_DELAY1 While adding support for New PMIC, developer need to update the API functionality for New PMIC device accordingly.
pPmicCoreHandle | [IN] PMIC Interface Handle |
pFsmDelayType | [IN] PFSM Delay Type Valid values: Pmic_Pfsm_Delay_Type |
pfsmDelay | [IN] Delay for PFSM |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmGetPfsmDelay | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
uint8_t | pFsmDelayType, | ||
uint8_t * | pPfsmDelay | ||
) |
API to read PFSM Delay.
Requirement: REQ_TAG(PDK-9136) Design: did_pmic_pfsm_cfg_readback
This function is used to read PFSM Delay Note: In this API, the default delay Type is assumed as PMIC_PFSM_DELAY1 While adding support for New PMIC, developer need to update the API functionality for New PMIC device accordingly.
pPmicCoreHandle | [IN] PMIC Interface Handle |
pFsmDelayType | [IN] PFSM Delay Type Valid values: Pmic_Pfsm_Delay_Type |
pPfsmDelay | [OUT] Pointer to store the Delay for PFSM |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |
int32_t Pmic_fsmSetNsleepSignalVal | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const bool | nsleepType, | ||
const uint8_t | nsleepVal | ||
) |
API to set PMIC Nsleep1B/2B Signal value.
Requirement: REQ_TAG(PDK-9146) Design: did_pmic_fsm_cfg_readback
This function is used to configure the Nsleep1B/2B signal level
pPmicCoreHandle | [IN] PMIC Interface Handle. |
nsleepType | [IN] NSLEEP signal Valid values: Pmic_Nsleep_Signals |
nsleepVal | [IN] PMIC Nsleep signal level High/Low to be configured. Valid values Pmic_Nsleep_SignalLvl |
int32_t Pmic_fsmGetNsleepSignalVal | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const bool | nsleepType, | ||
uint8_t * | pNsleepVal | ||
) |
API to get PMIC Nsleep1B/2B Signal value.
Requirement: REQ_TAG(PDK-9146) Design: did_pmic_fsm_cfg_readback
This function is used to read the signal level of the Nsleep1B/2B signal
pPmicCoreHandle | [IN] PMIC Interface Handle |
nsleepType | [IN] NSLEEP signal Valid values: Pmic_Nsleep_Signals |
pNsleepVal | [OUT] Pointer to store PMIC Nsleep signal level High/Low. Valid values Pmic_Nsleep_SignalLvl |
int32_t Pmic_fsmRecoverSocPwrErr | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | nsleepVal | ||
) |
API to recover from SOC Power Error using Nsleep1B and Nsleep2B signal.
Requirement: REQ_TAG(PDK-9123), REQ_TAG(PDK-9159), REQ_TAG(PDK-9329) Design: did_pmic_fsm_recover_soc_pwr_err
This function is used to recover from SOC Power Error without rebooting the system Note: Application need to call this API from MCU domain when SOC Power Error on Primary PMIC Step-1 - PMIC LLD has to configure NSLEEP2 & NSLEEP1 signals to ‘10’ Step-2 - Application has to wait for 9us Step-3 - PMIC LLD has to configure NSLEEP2 & NSLEEP1 signals to ‘11’
pPmicCoreHandle | [IN] PMIC Interface Handle |
nsleepVal | [IN] PMIC Nsleep signal level High/Low to be configured. Valid values Pmic_Nsleep_SignalLvl |
int32_t Pmic_fsmEnableI2cTrigger | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | i2cTriggerType, | ||
const uint8_t | i2cTriggerVal | ||
) |
API to initiate FSM I2C trigger for given FSM I2C trigger type.
Requirement: REQ_TAG(PDK-9330) Design: did_pmic_fsm_i2c_trigger
This function is used to to initiate FSM I2C trigger for given FSM I2C trigger type Note: In this API, the default i2cTriggerType is assumed as PMIC_FSM_I2C_TRIGGER0. While adding support for New PMIC device, developer need to update the API functionality for New PMIC device accordingly.
pPmicCoreHandle | [IN] PMIC Interface Handle |
i2cTriggerType | [IN] FSM I2C Trigger Type Valid values: Pmic_Fsm_I2c_Trigger_Type |
i2cTriggerVal | [IN] FSM I2C Trigger Value Valid values: Pmic_Fsm_I2c_Trigger_Val |
int32_t Pmic_fsmGetI2cTriggerVal | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | i2cTriggerType, | ||
uint8_t * | pI2cTriggerVal | ||
) |
API to get FSM I2C trigger Value for given FSM I2C trigger type.
Requirement: REQ_TAG(PDK-9330) Design: did_pmic_fsm_i2c_trigger
This function is used to read the FSM I2C trigger Value of the FSM Trigger Type
pPmicCoreHandle | [IN] PMIC Interface Handle |
i2cTriggerType | [IN] FSM I2C Trigger Type Valid values: Pmic_Fsm_I2c_Trigger_Type |
pI2cTriggerVal | [OUT] Pointer to store FSM I2C Trigger Value Valid values Pmic_Fsm_I2c_Trigger_Val |
int32_t Pmic_fsmRequestDdrGpioRetentionMode | ( | Pmic_CoreHandle_t * | pPmicCoreHandle, |
const uint8_t | retentionMode, | ||
const uint8_t | i2cTriggerVal | ||
) |
API to initiate DDR/GPIO Retention Mode.
Requirement: REQ_TAG(PDK-9563), REQ_TAG(PDK-9564) Design: did_pmic_ddr_gpio_retention_cfg
This function initiates a request to exercise DDR/GPIO Retention Mode on the device based on the Retention Mode Note: PMIC_FSM_GPIO_RETENTION_MODE is valid only for J7200 SOC In this API, the default SOC Type is assumed as J721E SOC While adding support for other SOCs, developer need to update the API functionality for New SOC device accordingly.
pPmicCoreHandle | [IN] PMIC Interface Handle |
retentionMode | [IN] Retention Mode Valid values: Pmic_Fsm_Retention_Mode PMIC_FSM_GPIO_RETENTION_MODE is valid only for J7200 SOC |
i2cTriggerVal | [IN] FSM I2C Trigger Value Valid values: Pmic_Fsm_I2c_Trigger_Val |
PMIC_ST_SUCCESS | in case of success or appropriate error code For valid values Pmic_ErrorCodes |