![]() |
PDK API Guide for J721E
|
Defines the structures / control operations that could be used to configure / control Graph of VPAC.
Go to the source code of this file.
Data Structures | |
struct | Fc_ErrEventParams |
Structure for error event parameters Used to register callback for the given set of events. More... | |
Typedefs | |
typedef void(* | fc_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
Prototype for the Error Event for Flex-connect. The callback for the Flex-connect error events can be registered using Fc_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs. More... | |