![]() |
PDK API Guide for J721E
|
GPIO driver.
============================================================================
The GPIO header file should be included in an application as follows:
The GPIO module allows you to manage General Purpose I/O pins via simple and portable APIs. GPIO pin behaviour can be configured completely statically, or dynamically defined at runtime.
The application is required to supply a device specific GPIOXXX_Config structure to the module. This structure communicates to the GPIO module how to configure the pins that will be used by the application (See the description of GPIO_PinConfig).
The application is required to call GPIO_init(). This function will initialize all the GPIO pins defined in the GPIO_PinConfig table to the configurations specified. Once that is completed the other APIs can be used to access the pins.
Asserts are used to verify that the driver has been initialized and to validate pin indexes within the various APIs.
See the device specific GPIO header file for configuration details.
Go to the source code of this file.
Data Structures | |
struct | GPIO_FxnTable |
The definition of a GPIO function table that contains the required set of functions to control a specific GPIO driver implementation. More... | |
struct | GPIO_Config |
GPIO Global configuration. More... | |
Macros | |
#define | GPIO_MAX_CONFIG_CNT (3U) |
GPIO_PinConfig pin direction configuration macros | |
#define | GPIO_CFG_OUTPUT (((uint32_t) 0) << GPIO_CFG_IO_LSB) /*! Pin is an output. */ |
#define | GPIO_CFG_OUT_STD (((uint32_t) 0) << GPIO_CFG_IO_LSB) /*! Output pin is not Open Drain */ |
#define | GPIO_CFG_OUT_OD_NOPULL (((uint32_t) 2) << GPIO_CFG_IO_LSB) /*! Output pin is Open Drain */ |
#define | GPIO_CFG_OUT_OD_PU (((uint32_t) 4) << GPIO_CFG_IO_LSB) /*! Output pin is Open Drain w/ pull up */ |
#define | GPIO_CFG_OUT_OD_PD (((uint32_t) 6) << GPIO_CFG_IO_LSB) /*! Output pin is Open Drain w/ pull dn */ |
#define | GPIO_CFG_OUT_HIGH (((uint32_t) 1) << GPIO_CFG_OUT_BIT) /*! Set pin's output to 1. */ |
#define | GPIO_CFG_OUT_LOW (((uint32_t) 0) << GPIO_CFG_OUT_BIT) /*! Set pin's output to 0. */ |
#define | GPIO_CFG_OUT_STR_LOW (((uint32_t) 0) << GPIO_CFG_OUT_STRENGTH_LSB) |
#define | GPIO_CFG_OUT_STR_MED (((uint32_t) 1) << GPIO_CFG_OUT_STRENGTH_LSB) |
#define | GPIO_CFG_OUT_STR_HIGH (((uint32_t) 2) << GPIO_CFG_OUT_STRENGTH_LSB) |
#define | GPIO_CFG_INPUT (((uint32_t) 1) << GPIO_CFG_IO_LSB) /*! Pin is an input. */ |
#define | GPIO_CFG_IN_NOPULL (((uint32_t) 1) << GPIO_CFG_IO_LSB) /*! Input pin has no PU/PD */ |
#define | GPIO_CFG_IN_PU (((uint32_t) 3) << GPIO_CFG_IO_LSB) /*! Input pin has Pullup */ |
#define | GPIO_CFG_IN_PD (((uint32_t) 5) << GPIO_CFG_IO_LSB) /*! Input pin has Pulldown */ |
GPIO_PinConfig pin interrupt configuration macros | |
#define | GPIO_CFG_IN_INT_NONE (((uint32_t) 0) << GPIO_CFG_INT_LSB) /*! No Interrupt */ |
#define | GPIO_CFG_IN_INT_FALLING (((uint32_t) 1) << GPIO_CFG_INT_LSB) /*! Interrupt on falling edge */ |
#define | GPIO_CFG_IN_INT_RISING (((uint32_t) 2) << GPIO_CFG_INT_LSB) /*! Interrupt on rising edge */ |
#define | GPIO_CFG_IN_INT_BOTH_EDGES (((uint32_t) 3) << GPIO_CFG_INT_LSB) /*! Interrupt on both edges */ |
#define | GPIO_CFG_IN_INT_LOW (((uint32_t) 4) << GPIO_CFG_INT_LSB) /*! Interrupt on low level */ |
#define | GPIO_CFG_IN_INT_HIGH (((uint32_t) 5) << GPIO_CFG_INT_LSB) /*! Interrupt on high level */ |
Special GPIO_PinConfig configuration macros | |
#define | GPIO_CFG_IN_INT_ONLY (((uint32_t) 1) << 27) /*! configure interrupt only */ |
'Or' in this GPIO_PinConfig definition to inform GPIO_setConfig() to only configure the interrupt attributes of a GPIO input pin. More... | |
#define | GPIO_DO_NOT_CONFIG 0x7fff0001U /*! Do not configure this Pin */ |
Use this GPIO_PinConfig definition to inform GPIO_init() NOT to configure the corresponding pin. More... | |
Typedefs | |
typedef uint32_t | GPIO_PinConfig |
GPIO pin configuration settings. More... | |
typedef void(* | GPIO_CallbackFxn) (void) |
GPIO callback function type. More... | |
typedef void(* | GPIO_InitFxn) (void) |
Initializes the GPIO module. More... | |
typedef uint32_t(* | GPIO_ReadFxn) (uint32_t idx) |
Reads the value of a GPIO pin. More... | |
typedef void(* | GPIO_WriteFxn) (uint32_t idx, uint32_t value) |
Writes the value to a GPIO pin. More... | |
typedef void(* | GPIO_clearIntFxn) (uint32_t idx) |
Clear a GPIO pin interrupt flag. More... | |
typedef void(* | GPIO_disableIntFxn) (uint32_t idx) |
Disable a GPIO pin interrupt. More... | |
typedef void(* | GPIO_enableIntFxn) (uint32_t idx) |
Enable a GPIO pin interrupt. More... | |
typedef void(* | GPIO_setCallbackFxn) (uint32_t idx, GPIO_CallbackFxn callback) |
Bind a callback function to a GPIO pin interrupt. More... | |
typedef void(* | GPIO_setConfigFxn) (uint32_t idx, GPIO_PinConfig pinConfig) |
Configure the gpio pin. More... | |
typedef void(* | GPIO_toggleFxn) (uint32_t idx) |
Toggles the current state of a GPIO. More... | |
typedef GPIO_Config | GPIOConfigList[GPIO_MAX_CONFIG_CNT] |
Functions | |
void | GPIO_clearInt (uint32_t idx) |
Clear a GPIO pin interrupt flag. More... | |
void | GPIO_disableInt (uint32_t idx) |
Disable a GPIO pin interrupt. More... | |
void | GPIO_enableInt (uint32_t idx) |
Enable a GPIO pin interrupt. More... | |
void | GPIO_init (void) |
Initializes the GPIO module. More... | |
uint32_t | GPIO_read (uint32_t idx) |
Reads the value of a GPIO pin. More... | |
void | GPIO_setCallback (uint32_t idx, GPIO_CallbackFxn callback) |
Bind a callback function to a GPIO pin interrupt. More... | |
void | GPIO_setConfig (uint32_t idx, GPIO_PinConfig pinConfig) |
Configure the gpio pin. More... | |
void | GPIO_toggle (uint32_t idx) |
Toggles the current state of a GPIO. More... | |
void | GPIO_write (uint32_t idx, uint32_t value) |
Writes the value to a GPIO pin. More... | |