Sqrtdp


Detailed Description


Functions

double sqrtdp (double a)
double sqrtdp_c (double a)


Function Documentation

double sqrtdp ( double  a  ) 

Description:
The sqrtdp function returns the square root function of a real floating-point argument a. The return value is the square root value of a.
Parameters:
[in] a = Input double
Returns:
Resultant double
Special Cases:
  • If a <= 0, the return value is zero for C/Inline/Vector and rsqrt(|a|) for Asm.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double sqrtdp_c ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated