Sinhdp


Detailed Description


Functions

double sinhdp_c (double a)
double sinhdp (double a)


Function Documentation

double sinhdp_c ( double  a  ) 

Description:
The sinhdp function returns the hyperbolic sine function of a real floating-point argument a. If the magnitude of a is too large, infinity is returned.
Parameters:
[in] a = Input double
Returns:
Resultant double
Special Cases:
  • If a > +710.475860073944, then the return value is INF
  • If a < -710.475860073944, then the return value is -INF.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double sinhdp ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated