Logsp


Detailed Description


Functions

float logsp (float a)
float logsp_c (float a)


Function Documentation

float logsp ( float  a  ) 

Description:
The logsp function returns the logarithm function of a real floating-point argument a. The return value is the base e logarithmic value of a.
Parameters:
[in] a = Input float
Returns:
Resultant float
Special Cases:
  • If a is Inf, the return value is 88.99999 (Asm) or 709.7827 (C/Inline/Vector).
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

float logsp_c ( float  a  ) 


Copyright 2016, Texas Instruments Incorporated