Logdp


Detailed Description


Functions

double logdp (double a)
double logdp_c (double a)


Function Documentation

double logdp ( double  a  ) 

Description:
The logdp function returns the logarithm function of a real floating-point argument a. The return value is the base e logarithmic value of a.
Parameters:
[in] a = Input double
Returns:
Resultant double
Special Cases:
  • If a is NaN (Not a Number), the return value may be random.
  • If a <= 0, the return value is -inf.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double logdp_c ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated