Divdp


Detailed Description


Functions

double divdp (double a, double b)
double divdp_c (double a, double b)


Function Documentation

double divdp ( double  a,
double  b 
)

Description:
The divdp_v function returns the division function of a real floating-point argument a by b. The return value is the number resulting from a/b.
Parameters:
[in] a = Input double dividend
[in] b = Input double divisor
Returns:
Resultant double
Special Cases:
  • If | b | < 2.225e-308, then the return value is NaN.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double divdp_c ( double  a,
double  b 
)


Copyright 2016, Texas Instruments Incorporated