Cosdp


Detailed Description


Functions

double cosdp (double a)
double cosdp_c (double a)


Function Documentation

double cosdp ( double  a  ) 

Description:
The cosdp function returns the cosine of a floating-point argument a. The angle a is expressed in radians. The return value is in the range of [-1.0 and +1.0]. An argument with a large magnitude may produce a result with little or no significance.
Parameters:
[in] a = Input double
Returns:
Resultant double
Special Cases:
  • If | a | > 1.0737e+9, then the return value is zero for large angles.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double cosdp_c ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated