Asindp


Detailed Description


Functions

double asindp_c (double a)
double asindp (double a)


Function Documentation

double asindp_c ( double  a  ) 

Description:
The asindp function returns the arc sine of a floating-point argument a. The return value is an angle in the range [-PI/2, PI/2] radians.
Parameters:
[in] a = Input float
Returns:
Resultant float
Special Cases:
  • If a is not in the range [-1, 1], the return value is NaN (Not a Number).
  • If a is NaN, the return value is NaN.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

double asindp ( double  a  ) 


Copyright 2016, Texas Instruments Incorporated