Acossp


Detailed Description


Functions

float acossp_c (float a)
float acossp (float a)


Function Documentation

float acossp_c ( float  a  ) 

Description:
The acossp function returns the arc cosine of a floating-point argument a. The return value is an angle in the range [0, PI] radians.
Parameters:
[in] a = Input float
Returns:
Resultant float
Special Cases:
  • If a is not in the range [-1, 1], the return value is NaN (Not a Number).
  • If a is NaN, the return value is NaN.
See also:
Implementation Notes:
  • The code supports both big and little endian modes.

float acossp ( float  a  ) 


Copyright 2016, Texas Instruments Incorporated