![]() |
TI J721E Imaging User Guide
|
tivx_aewb_config_t parameters
Data Fields | |
uint16_t | sensor_dcc_id |
uint8_t | sensor_img_format |
uint8_t | sensor_img_phase |
uint8_t | awb_mode |
uint8_t | ae_mode |
uint8_t | awb_num_skip_frames |
uint8_t | ae_num_skip_frames |
uint8_t | channel_id |
uint16_t tivx_aewb_config_t::sensor_dcc_id |
DCC ID of the sensor. Must correspond to the value specified in tuning XML files
uint8_t tivx_aewb_config_t::sensor_img_format |
Image Format : BAYER = 0x0, Rest unsupported
uint8_t tivx_aewb_config_t::sensor_img_phase |
Image Format : BGGR = 0, GBRG = 1, GRBG = 2, RGGB = 3
uint8_t tivx_aewb_config_t::awb_mode |
AWB Mode : 0 = Auto, 1 = Manual, 2 = Disabled
uint8_t tivx_aewb_config_t::ae_mode |
AE Mode : 0 = Auto, 1 = Manual, 2 = Disabled
uint8_t tivx_aewb_config_t::awb_num_skip_frames |
0 = Process every frame
uint8_t tivx_aewb_config_t::ae_num_skip_frames |
0 = Process every frame
uint8_t tivx_aewb_config_t::channel_id |
channel ID