![]() |
PDK API Guide for J721E
|
UDMA OSAL related parameters and API.
Go to the source code of this file.
Data Structures | |
struct | Udma_OsalPrms |
UDMA driver OSAL function pointers. More... | |
struct | Udma_OsalCachePrms |
UDMA driver OSAL cache function pointers. More... | |
Typedefs | |
typedef uintptr_t(* | Udma_OsalDisableAllIntrFxn) (void) |
UDMA OSAL intr disable function prototype. More... | |
typedef void(* | Udma_OsalRestoreAllIntrFxn) (uintptr_t cookie) |
UDMA OSAL intr restore function prototype. More... | |
typedef void(* | Udma_OsalDisableIntrFxn) (uint32_t coreIntrNum) |
UDMA OSAL intr disable function prototype. More... | |
typedef void *(* | Udma_OsalMutexCreateFxn) (void) |
UDMA OSAL mutex create function prototype to protect critical section. More... | |
typedef void(* | Udma_OsalMutexDeleteFxn) (void *mutexHandle) |
UDMA OSAL mutex delete function prototype. More... | |
typedef void(* | Udma_OsalMutexLockFxn) (void *mutexHandle) |
UDMA OSAL mutex lock function prototype. More... | |
typedef void(* | Udma_OsalMutexUnlockFxn) (void *mutexHandle) |
UDMA OSAL mutex lock function prototype. More... | |
typedef void(* | Udma_OsalIsrFxn) (uintptr_t arg) |
UDMA OSAL ISR callback function prototype. More... | |
typedef void *(* | Udma_OsalRegisterIntrFxn) (Udma_OsalIsrFxn isrFxn, uint32_t coreIntrNum, uint32_t intrPriority, void *arg) |
UDMA OSAL ISR register function prototype. More... | |
typedef void(* | Udma_OsalUnRegisterIntrFxn) (void *hwiHandle) |
UDMA OSAL ISR unregister function prototype. More... | |
typedef void(* | Udma_OsalCacheInv) (const void *addr, int32_t size) |
UDMA OSAL cache invalidate function prototype. More... | |
typedef void(* | Udma_OsalCacheWb) (const void *addr, int32_t size) |
UDMA OSAL cache writeback function prototype. More... | |
Functions | |
int32_t | Udma_osalSetCachePrms (const Udma_OsalCachePrms *cachePrms) |
This API sets the OSAL cache paramaters incase user needs to override the default cache API. More... | |
void | UdmaOsalPrms_init (Udma_OsalPrms *osalPrms) |
Udma_OsalPrms structure init function. More... | |
void | UdmaOsalCachePrms_init (Udma_OsalCachePrms *cachePrms) |
Udma_OsalCachePrms structure init function. More... | |