PDK API Guide for J721E
|
Set the desired state of the device.
Certain flags can also be set to alter the device state: TISCI_MSG_FLAG_DEVICE_WAKE_ENABLED, TISCI_MSG_FLAG_DEVICE_RESET_ISO, TISCI_MSG_FLAG_DEVICE_EXCLUSIVE
hdr | TISCI header |
id | Indicates which device to modify |
reserved | Field is ignored |
state | The desired state of the device. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | id |
uint32_t | reserved |
uint8_t | state |
struct tisci_header tisci_msg_set_device_req::hdr |
uint32_t tisci_msg_set_device_req::id |
uint32_t tisci_msg_set_device_req::reserved |
uint8_t tisci_msg_set_device_req::state |