![]() |
PDK API Guide for J721E
|
Configures a Navigator Subsystem UDMAP global configuration region. Configures the non-real-time registers of a Navigator Subsystem UDMAP global configuration region. The GCFG region being programmed must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment array. Individual fields for registers specified as valid are not checked for correctness. It is the application's responsibility to verify if the register fields are being set according to the device specification.
hdr | Standard TISCI header |
valid_params | Bitfield defining validity of global configuration parameters. The configuration fields are not valid, and will not be used for global configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for tisci_msg_rm_udmap_gcfg_cfg_req::perf_ctrl 1 - Valid bit for tisci_msg_rm_udmap_gcfg_cfg_req::emu_ctrl 2 - Valid bit for tisci_msg_rm_udmap_gcfg_cfg_req::psil_to 3 - Valid bit for tisci_msg_rm_udmap_gcfg_cfg_req::rflowfwstat |
nav_id | SoC device ID of Navigator Subsystem where global configuration is located |
perf_ctrl | Configures the performance control register. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_GCFG_PERF_CTRL_VALID is set in tisci_msg_rm_udmap_gcfg_cfg_req::valid_params. |
emu_ctrl | Configures the emulation control register. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_GCFG_EMU_CTRL_VALID is set in tisci_msg_rm_udmap_gcfg_cfg_req::valid_params. |
psil_to | Configures the PSI-L proxy timeout register. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_GCFG_PSIL_TO_VALID is set in tisci_msg_rm_udmap_gcfg_cfg_req::valid_params. |
rflowfwstat | Writes the rx flow ID firewall status register. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_GCFG_RFLOWFWSTAT_VALID is set in tisci_msg_rm_udmap_gcfg_cfg_req::valid_params. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | valid_params |
uint16_t | nav_id |
uint32_t | perf_ctrl |
uint32_t | emu_ctrl |
uint32_t | psil_to |
uint32_t | rflowfwstat |
struct tisci_header tisci_msg_rm_udmap_gcfg_cfg_req::hdr |
uint32_t tisci_msg_rm_udmap_gcfg_cfg_req::valid_params |
uint16_t tisci_msg_rm_udmap_gcfg_cfg_req::nav_id |
uint32_t tisci_msg_rm_udmap_gcfg_cfg_req::perf_ctrl |
uint32_t tisci_msg_rm_udmap_gcfg_cfg_req::emu_ctrl |
uint32_t tisci_msg_rm_udmap_gcfg_cfg_req::psil_to |
uint32_t tisci_msg_rm_udmap_gcfg_cfg_req::rflowfwstat |