![]() |
PDK API Guide for J721E
|
Delegates the specified flow to another host for configuration. Only the original owner of the flow, as specified in the RM board configuration resource entries, can delegate an additional host as able to configure the flow. A flow's delegation can be cleared by the original owner of the flow using the clear parameter.
hdr | Standard TISCI header |
valid_params | Bitfield defining validity of flow delegation parameters. The flow delegation fields are not valid, and will not be used, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for tisci_msg_rm_udmap_flow_delegate_req::delegated_host 1 - Valid bit for tisci_msg_rm_udmap_flow_delegate_req::clear |
dev_id | SoC device ID of DMA in which the common flow exists. |
flow_index | DMA common flow being delegated for configuration. |
delegated_host | The host delegated configuration access to the flow. The host must be a valid host within the SoC. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_HOST_VALID is set in tisci_msg_rm_udmap_flow_delegate_req::valid_params. |
clear | Clears the flow delegation when enabled. Set this parameter to TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_CLEAR. This field is only valid if TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_CLEAR_VALID is set in tisci_msg_rm_udmap_flow_delegate_req::valid_params. |
Data Fields | |
struct tisci_header | hdr |
uint32_t | valid_params |
uint16_t | dev_id |
uint16_t | flow_index |
uint8_t | delegated_host |
uint8_t | clear |
struct tisci_header tisci_msg_rm_udmap_flow_delegate_req::hdr |
uint32_t tisci_msg_rm_udmap_flow_delegate_req::valid_params |
uint16_t tisci_msg_rm_udmap_flow_delegate_req::dev_id |
uint16_t tisci_msg_rm_udmap_flow_delegate_req::flow_index |
uint8_t tisci_msg_rm_udmap_flow_delegate_req::delegated_host |
uint8_t tisci_msg_rm_udmap_flow_delegate_req::clear |