This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
System Firmware TISCI RM Proxy Messaging
TISCI Protocol Definitions for proxy messagesConfigures a Navigator Subsystem proxy
Configures the channelized firewalls of a Navigator Subsystem proxy. The firewalls are configured to all the header host access to the backing RAM and target data configuration registers. The proxy index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.
- Parameters
-
hdr | Standard TISCI header |
valid_params | Bitfield defining validity of proxy configuration parameters. This field is unused at the moment but exists if expansion of the API is needed in the future. |
nav_id | SoC device ID of Navigator Subsystem where proxy is located |
index | Proxy index. |