![]() |
PDK API Guide for J721E
|
Result of a query operation.
hdr | TISCI header |
freq_hz | The frequency in Hz that the hardware would set for the given parameters. |
Data Fields | |
struct tisci_header | hdr |
uint64_t | freq_hz |
struct tisci_header tisci_msg_query_freq_resp::hdr |
uint64_t tisci_msg_query_freq_resp::freq_hz |