![]() |
PDK API Guide for J721E
|
Companding Lut configuration Structure LUT based companding is used at many places in RAWFE This structure is common and used for configuring these Luts.
struct Vhwa_LutConfig
Data Fields | |
uint32_t | enable |
uint32_t | inputBits |
uint32_t | clip |
uint32_t * | tableAddr |
uint32_t Vhwa_LutConfig::enable |
Flag to enable Lut
uint32_t Vhwa_LutConfig::inputBits |
Number of input bits
uint32_t Vhwa_LutConfig::clip |
Output Clip value
uint32_t* Vhwa_LutConfig::tableAddr |
Pointer to the Lut Address, must not be null if enable is set to TRUE