![]() |
PDK API Guide for J721E
|
Bandwith limiter configuration for HTS. This is used to slowed down the HTS by introducing clock cycles between internal start signals. These are advanced parameters and should not be modified in most cases.
struct Vhwa_HtsLimiter
Data Fields | |
uint32_t | enableBwLimit |
uint32_t | cycleCnt |
uint32_t | tokenCnt |
uint32_t Vhwa_HtsLimiter::enableBwLimit |
Enable Bandwidth Limiter
uint32_t Vhwa_HtsLimiter::cycleCnt |
Average Cycle count between successive Thread Start
uint32_t Vhwa_HtsLimiter::tokenCnt |
Max Token count to create average BW