![]() |
PDK API Guide for J721E
|
UDMA proxy object.
UDMA proxy handle.
Note: This is an internal/private driver structure and should not be used or modified by caller.
Data Fields | |
Udma_DrvHandle | drvHandle |
uint16_t | proxyNum |
uintptr_t | proxyAddr |
uint32_t | proxyInitDone |
Udma_DrvHandle Udma_ProxyHandle::drvHandle |
Pointer to global driver handle.
uint16_t Udma_ProxyHandle::proxyNum |
Proxy number
uintptr_t Udma_ProxyHandle::proxyAddr |
Proxy address for push/pop ring operation through proxy
uint32_t Udma_ProxyHandle::proxyInitDone |
Flag to set the proxy object is init.