![]() |
PDK API Guide for J721E
|
UDMAP receive flow id firewall status.
This structure contains status information collected whenever the receive flow ID firewall detects a flow ID that is out of range for an incoming packet.
Data Fields | |
uint32_t | isException |
uint32_t | flowId |
uint32_t | chNum |
uint32_t Udma_EventRxFlowIdFwStatus::isException |
This is set whenever the Flow ID firewall detects a Flow ID is out of range for an incoming packet.
uint32_t Udma_EventRxFlowIdFwStatus::flowId |
[OUT] The flow ID that was received on the trapped packet
uint32_t Udma_EventRxFlowIdFwStatus::chNum |
[OUT] The channel index on which the trapped packet was received