validParams | Selection of structure parameters to be set from the combination of the Pmic_WdgCfgValidParamBitPos and the corresponding member value will be updated. |
longWinDuration_ms | Long Window duration in milli seconds. To get more effective results user has to program long window with multiples of 3000. For PG1.0, the valid range is (100, 3000, 6000, 9000,....12000, ..., 765000). For PG2.0, the valid range is (80, 125, 250, 375,....8000, 12000, 16000, 20000 ..., 772000). |
win1Duration_us | Window-1 duration in Micro Seconds. To get more effective results user has to program window1 with multiples of 550. The valid range is (550, 1100, 1650, 2200, 2750, ..., 70400). |
win2Duration_us | Window-2 duration in Micro Seconds. To get more effective results user has to program window1 with multiples of 550. The valid range is (550, 1100, 1650, 2200, 2750, ..., 70400). |
failThreshold | Fail threshold value. For valid Values: Pmic_WdgFailThresholdCount. |
rstThreshold | Reset threshold Value. For valid Values: Pmic_WdgResetThresholdCount. |
wdgMode | Value to set watchdog mode. For valid Values: Pmic_WdgTriggerQAMode. |
pwrHold | Value to Enable or disable watchdog pwrHold. For valid Values: Pmic_WdgPwrHoldEnDisable. |
rstEnable | To enable or diable warm reset on fail. For valid Values: Pmic_WdgResetEnDisable. |
retLongWin | To enable or disable return to long window after completion of the curent sequence. For valid Values: Pmic_WdgReturnLongWinEnDisable. |
qaFdbk | Configure QA feed back value. For valid Values: Pmic_WdgQaFdbkVal. |
qaLfsr | Configure QA LFSR value. For valid Values: Pmic_WdgQaLfsrVal. |
qaQuesSeed | Configure QA question seed value. For valid Values: Pmic_WdgQaQuestionSeedVal. |