RTC Date configuration. The Pmic_RtcDate_s structure contains set of date parameters to set/get the RTC Date.
- Parameters
-
validParams | Validate params Bits. Depending on the parameters want to get/set, corresponding bits should be set in validParam. |
day | Value to represent the day. Valid only when PMIC_RTC_DATE_CFG_DAY_VALID bit of validParams is set. |
month | Value to represent the Month. For valid values Pmic_RtcMonth. Valid only when PMIC_RTC_DATE_CFG_MONTH_VALID bit of validParams is set. |
year | Value to represent the Year. Valid only when PMIC_RTC_DATE_CFG_YEAR_VALID bit of validParams is set. |
weekday | Value to represent the weekday of the week. For Valid Values: Pmic_RtcWeekDay. Valid only when PMIC_RTC_DATE_CFG_WEEKDAY_VALID bit of validParams is set. |