Power configuration The power control and config structure Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
- Parameters
-
validParams | Selection of structure parameters to be set, from the combination of Pmic_PowerCommonParamCfg and the corresponding member value must be updated |
pgoodWindow | Select the type of voltage monitoring for PGOOD signal For valid values Pmic_Power_Good_Window Valid only when PMIC_POWER_PGOOD_WINDOW_VALID bit set. |
pgoodPolarity | Select the PGOOD signal polarity For valid values Valid values Pmic_Power_Good_Polarity Valid only when PMIC_POWER_PGOOD_POL_VALID bit is set. |
deglitchTimeSel | Deglitch time select for all power resources Valid values for TPS6594x Leo Device Valid only for TPS6594x Leo PMIC PG2.0 Pmic_TPS6594x_Vmon_DeglitchTime_Sel. Valid values for LP8764x HERA Device Valid for both LP8764x Hera PMIC PG1.0 and PG2.0 Pmic_LP8764x_Vmon_DeglitchTime_Sel. Valid only when PMIC_CFG_DEGLITCH_TIME_SEL_VALID bit is set. |
severeErrorTrig | Select the trigger selection for severe Error For valid values Pmic_Power_Trigger_Sel Valid only when PMIC_SEVERE_ERR_TRIG_VALID bit set. |
otherRailTrig | Select the trigger selection for other rail group For valid values Pmic_Power_Trigger_Sel Valid only when PMIC_OTHER_RAIL_TRIG_VALID bit set. |
socRailTrig | Select the trigger selection for soc rail group For valid values Pmic_Power_Trigger_Sel Valid only when PMIC_SOC_RAIL_TRIG_VALID bit set. |
mcuRailTrig | Select the trigger selection for mcu rail group For valid values Pmic_Power_Trigger_Sel Valid only when PMIC_MCU_RAIL_TRIG_VALID bit set. |
moderateRailTrig | Select the trigger selection for Moderate Error For valid values Pmic_Power_Trigger_Sel Valid only when PMIC_MODERATE_ERR_TRIG_VALID bit set |