PMIC Miscellaneous control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
- Parameters
-
validParams | Selection of structure parameters to be set, from the combination of Pmic_MiscCtrlValidParamCfg and the corresponding member value must be updated. Valid values Pmic_MiscCtrlValidParamCfg |
amuxOutRefOutEn | Enable/Disable Band gap Voltage to AMUX OUT Pin (for TPS6594x Leo Device) or RFF OUT Pin (for LP8764x Leo Device) Valid only when PMIC_CFG_AMUX_OUT_REF_OUT_EN_VALID bit is set Valid values Pmic_Tps6594xLeo_AMuxOutPinCtrl_Cfg (for TPS6594x Leo Device) Pmic_Lp8764xHera_RefOutPinCtrl_Cfg (for LP8764x Hera Device) |
clkMonEn | Enable or Disable internal Clock Monitoring Valid only when PMIC_CFG_CLK_MON_EN_VALID bit is set. Valid values Pmic_InternalClkMonitor_Cfg |
syncClkOutFreqSel | Selects SYNCCLKOUT Frequency Valid values Pmic_SyncClkOut_Freq_Sel Valid only when PMIC_CFG_SYNC_CLK_OUT_FREQ_SEL_VALID bit is set |
extClkSel | External clock Selection Valid values Pmic_ExtClk_Sel Valid only when PMIC_CFG_EXT_CLK_SEL_VALID bit is set. |
syncClkInFreq | Selects External clock Frequency Valid only when PMIC_CFG_SYNC_CLK_IN_FREQ_VALID bit is set. Valid values Pmic_Tps6594xLeo_ExtClk_Freq_Sel (for TPS6594x Leo Device) Pmic_Lp8764xHera_ExtClk_Freq_Sel (for LP8764x Hera Device) |
nRstOutSocSignal | Configure NRSTOUT_SOC Signal Note: When Application configures nRstOutSocSignal as PMIC_PIN_SIGNAL_LEVEL_LOW then SOC will be in reset Valid only when PMIC_CFG_NRSTOUT_SOC_VALID bit is set. Valid values Pmic_SignalLvl |
nRstOutSignal | Configure NRSTOUT Signal Note: When Application configures nRstOutSignal as PMIC_PIN_SIGNAL_LEVEL_LOW then MCU will be in reset Valid only when PMIC_CFG_NRSTOUT_VALID bit is set. Valid values Pmic_SignalLvl |