PMIC common control param configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
- Parameters
-
validParams | Selection of structure parameters to be set, from the combination of Pmic_CommonCtrlValidParamCfg and the corresponding member value must be updated Valid values Pmic_CommonCtrlValidParamCfg |
sreadSpectrumEn | Spread Spectrum Enable Value Valid only when PMIC_CFG_SPREAD_SPECTRUM_EN_VALID bit is set Valid values Pmic_SpreadSpectrum_Cfg |
skipEepromLoadEn | Enable/Disable to skip EEPROM defaults load on conf registers when device transition from Lpstandby to INIT state Valid only for LP8764x Hera Device Valid only when PMIC_CFG_SKIP_EEPROM_LOAD_VALID bit is set. Valid values Pmic_Lp8764xHera_Skip_EepromDef_LdCfg |
eepromDefaultLoad | Load/Not Loaded from EEPROM defaults on RTC domain Registers (for TPS6594x Leo Device) when device transition from Lpstandby/SafeRecovery to INIT state Enable/Disable load from EEPROM defaults on conf registers when skipEepromLoadEn = 0 when device transition from Lpstandby to INIT state Load/Not Loaded load from EEPROM defaults on conf registers when device transition from SafeRecovery to INIT state.Doesn't depends on skipEepromLoadEn Value (for LP8764x Hera Device) Valid only when PMIC_CFG_EEPROM_DEFAULT_VALID bit is set. Valid values Pmic_Tps6594xLeo_EepromDef_LdCfg (for TPS6594x Leo Device) Pmic_Lp8764xHera_EepromDef_LdCfg (for LP8764x Hera Device) |
enDrv | Control of ENABLE_DRV pin. Can be configured only When forceEnDrvLow set to 0 else ENABLE_DRV pin is set to PMIC_PIN_SIGNAL_LEVEL_LOW. Valid values Pmic_SignalLvl Valid only when PMIC_CFG_ENABLE_DRV_VALID bit is set. |
regLock | Register Lock configuration Valid values Pmic_RegisterLock_Config Valid only when PMIC_CFG_REG_LOCK_VALID bit is set Valid only for Pmic_setCommonCtrlConfig API |
spreadSpectrumDepth | Spread Spectrum modulation Depth Value Valid values Pmic_SpreadSpectrum_Mod_Depth_Sel Valid only when PMIC_CFG_SPREAD_SPECTRUM_DEPTH_VALID bit is set. |