PMIC Backup Battery control param Configuration Note: validParams is input param for all Set and Get APIs. other params except validParams is input param for Set APIs and output param for Get APIs.
- Parameters
-
validParams | Selection of structure parameters to be set, from the combination of Pmic_BatteryCtrlValidParamCfg and the corresponding member value must be updated. |
chargingEn | Enable/Disable Backup Battery Charging Valid only when PMIC_CFG_CHARGING_EN_VALID bit is set. Valid only for TPS6594x Leo Device Valid values Pmic_Tps6594xLeo_BatteryCharging_Cfg |
endOfChargeVoltage | Backup Battery configuration for End of charge Voltage Valid only when PMIC_CFG_END_OF_CHARGE_VOLTAGE_VALID bit is set. Valid only for TPS6594x Leo Device Valid values Pmic_Tps6594xLeo_EndOfChargeVoltage_Sel |
chargeCurrent | Backup Battery charging current value Valid only when PMIC_CFG_CHARGE_CURRENT_VALID bit is set. Valid only for TPS6594x Leo Device Valid values Pmic_Tps6594xLeo_Charging_Current_Sel |