![]() |
PDK API Guide for J721E
|
structure to hold the error condition and the status
This is the structure which holds the error condition and also the error status. Depending on the error status the application can take the decision to recover from the error
Data Fields | |
bool | isDMAErr |
bool | isRcvOvrRunOrTxUndRunErr |
bool | isClkFailErr |
bool | isSyncErr |
uint32_t | retVal |
bool Mcasp_errCbStatus::isDMAErr |
DMA Error
bool Mcasp_errCbStatus::isRcvOvrRunOrTxUndRunErr |
Receive OverRun on Transmir UnderRun Error
bool Mcasp_errCbStatus::isClkFailErr |
Clock Fail Error
bool Mcasp_errCbStatus::isSyncErr |
Sync Error
uint32_t Mcasp_errCbStatus::retVal |
return value