![]() |
PDK API Guide for J721E
|
ICSSG TimeSync object.
Data Fields | |
EnetMod_Obj | enetMod |
void * | hIcssg |
int32_t | drift |
uint32_t | syncInterval |
volatile bool | setClockOngoing |
IcssgTimeSync_ClkType | clkType |
EnetMod_Obj IcssgTimeSync_Obj::enetMod |
EnetMod must be the first member
void* IcssgTimeSync_Obj::hIcssg |
ICSSG handle. Required internally cycleTime value
int32_t IcssgTimeSync_Obj::drift |
Drift applied on WC timers per sync interval. Workaround for rate computation
uint32_t IcssgTimeSync_Obj::syncInterval |
Sync Interval for drift applied on WC timers. Workaround for rate computation
volatile bool IcssgTimeSync_Obj::setClockOngoing |
Flag to indicate setClock is in progress
IcssgTimeSync_ClkType IcssgTimeSync_Obj::clkType |
Control variable for set/get operations - WC, ST