![]() |
PDK API Guide for J721E
|
TAS List Structure based on firmware memory map.
Data Fields | |
uint8_t | gateMaskList [ENET_TAS_MAX_CMD_LISTS] |
uint32_t | windowEndTimeList [ENET_TAS_MAX_CMD_LISTS] |
uint32_t | gateCloseTimeList [ENET_TAS_MAX_CMD_LISTS][ENET_TAS_MAX_NUM_QUEUES] |
uint8_t IcssgTas_FwList::gateMaskList[ENET_TAS_MAX_CMD_LISTS] |
Window gate mask list
uint32_t IcssgTas_FwList::windowEndTimeList[ENET_TAS_MAX_CMD_LISTS] |
Window end time list
uint32_t IcssgTas_FwList::gateCloseTimeList[ENET_TAS_MAX_CMD_LISTS][ENET_TAS_MAX_NUM_QUEUES] |
Array of gate close time for each queue in each window