![]() |
PDK API Guide for J721E
|
Enet UDMA TX Protocol Info structure.
It contains IPv4/IPv6 protcol information including checksum. This is copied to the CPPI RX control word (UDMA channel protocol specific info).
Data Fields | |
uint16_t | chkSumResOffset |
uint16_t | chkSumStartByte |
bool | chkSumInv |
uint16_t | chkSumByteCnt |
uint16_t EnetUdma_TxProtoInfo::chkSumResOffset |
Checksum result location - packet byte number where the checksum result will be placed in the outgoing packet. The first packet byte which is the first byte of the destination address is Byte 1
uint16_t EnetUdma_TxProtoInfo::chkSumStartByte |
Checksum start byte - packet byte number to start the checksum calculation on. The first packet byte is Byte 1
bool EnetUdma_TxProtoInfo::chkSumInv |
Flag to insert invalid checksum. When true a zero checksum value will be inverted and sent as FFFFh
uint16_t EnetUdma_TxProtoInfo::chkSumByteCnt |
Checksum byte count - number of bytes to calculate the checksum on. The outgoing Ethernet packet will have a checksum inserted when this value is non-zero