![]() |
PDK API Guide for J721E
|
RX resources.
Data Fields | |
uint32_t | internalAllocCoreId |
uint32_t | internalAllocCount |
uint32_t | resCnt |
EnetRm_CoreResTbl_t | rxResTbl |
EnetRm_ResEntry_t | rxRes [ENET_CFG_RM_RX_CH_MAX] |
uint32_t EnetRm_RxFlowIdxObj::internalAllocCoreId |
Core id of the owner of the internal RX channel
uint32_t EnetRm_RxFlowIdxObj::internalAllocCount |
Internal allocation counter
uint32_t EnetRm_RxFlowIdxObj::resCnt |
Resource count
EnetRm_CoreResTbl_t EnetRm_RxFlowIdxObj::rxResTbl |
RX resource table for all applicable cores
EnetRm_ResEntry_t EnetRm_RxFlowIdxObj::rxRes[ENET_CFG_RM_RX_CH_MAX] |
RX resource entries