![]() |
PDK API Guide for J721E
|
Structure containing DSS parameters. This structure is used as an argument to IOCTL_DSS_DISP_SET_DSS_PARAMS.
Data Fields | |
CSL_DssVidPipeCfg | pipeCfg |
CSL_DssVidPipeDmaCfg | dmaCfg |
CSL_DssVidPipeAlphaCfg | alphaCfg |
CSL_DssVidPipeVC1Cfg | vc1Cfg |
Dss_DispPipeCropParams | cropParams |
Fvid2_PosConfig | layerPos |
CSL_DssVidPipeCfg Dss_DispParams::pipeCfg |
Video pipeline configuration
CSL_DssVidPipeDmaCfg Dss_DispParams::dmaCfg |
Video pipeline DMA configuration
CSL_DssVidPipeAlphaCfg Dss_DispParams::alphaCfg |
Video pipeline alpha configuration
CSL_DssVidPipeVC1Cfg Dss_DispParams::vc1Cfg |
Video pipeline VC1 configuration
Dss_DispPipeCropParams Dss_DispParams::cropParams |
Video pipeline Crop parameters, used only for J7 platform
Fvid2_PosConfig Dss_DispParams::layerPos |
Position of the video buffer described using Fvid2_PosConfig
startX:
X position of the video buffer The first pixel on the left of the screen has the X-position 0
startY:
Y position of the video buffer The line at the top has the Y-position 0