![]() |
PDK API Guide for J721E
|
Structure containing current status of the display driver. This structure is used as an argument to IOCTL_DSS_DISP_GET_CURRENT_STATUS.
Data Fields | |
uint32_t | queueCount |
uint32_t | dequeueCount |
uint32_t | dispFrmCount |
uint32_t | repeatFrmCount |
uint32_t | underflowCount |
uint32_t | safetyViolationCount |
uint32_t Dss_DispCurrentStatus::queueCount |
Counter to keep track of how many requests are queued to the driver. Note: This counter will be reset at the time of driver create
uint32_t Dss_DispCurrentStatus::dequeueCount |
Counter to keep track of how many requests are dequeued from the driver. Note: This counter will be reset at the time of driver create
uint32_t Dss_DispCurrentStatus::dispFrmCount |
Counter to keep track of how many frames are displayed. For interlaced display, this is half of the actual field display. Note: This counter will be reset at the time of display start
uint32_t Dss_DispCurrentStatus::repeatFrmCount |
Counter to keep track of how many frames are repeated when the application fails to queue buffer at the display rate. Note: This counter will be reset at the time of display start
uint32_t Dss_DispCurrentStatus::underflowCount |
Counter to keep track of number of underflows Note: This counter will be reset at the time of driver create
uint32_t Dss_DispCurrentStatus::safetyViolationCount |
Counter to keep track of number of safety violations Note: This counter will be reset at the time of driver create