![]() |
PDK API Guide for J721E
|
Structure containing create status for the display driver. This should be passed as a status argument while creating the driver.
Data Fields | |
int32_t | retVal |
uint32_t | standard |
uint32_t | dispWidth |
uint32_t | dispHeight |
uint32_t | minNumPrimeBuf |
int32_t Dss_DispCreateStatus::retVal |
Return status of create call
uint32_t Dss_DispCreateStatus::standard |
Video Port standard like 1080p, 720p, etc. to which the video pipe is connected. For valid values see Fvid2_Standard
uint32_t Dss_DispCreateStatus::dispWidth |
Width of the display at the Video Port in pixels
uint32_t Dss_DispCreateStatus::dispHeight |
Height of the display at the Video Port in lines
uint32_t Dss_DispCreateStatus::minNumPrimeBuf |
Minimum number of buffers to prime before starting display operation