![]() |
PDK API Guide for J721E
|
Structure containing Overlay layer information. This structure is used as an argument to IOCTL_DSS_DCTRL_SET_LAYER_PARAMS.
Data Fields | |
uint32_t | overlayId |
uint32_t | pipeLayerNum [CSL_DSS_VID_PIPE_ID_MAX] |
uint32_t Dss_DctrlOverlayLayerParams::overlayId |
Overlay Id. See CSL_DssOverlayId for values
uint32_t Dss_DctrlOverlayLayerParams::pipeLayerNum[CSL_DSS_VID_PIPE_ID_MAX] |
Layer to which a particular Video Pipe Id is connected. For valid values see CSL_DssOverlayLayerNum