![]() |
PDK API Guide for J721E
|
Data Fields | |
int32_t | numChannels |
int32_t | contextSize |
int32_t | traceLogLevel |
int32_t(* | DmaUtilsVprintf )(const char *format, va_list arg) |
Udma_DrvHandle | udmaDrvHandle |
int32_t DmaUtilsAutoInc3d_InitParam::numChannels |
DRU queue number to which a particular channel should submit its transfers
int32_t DmaUtilsAutoInc3d_InitParam::contextSize |
Owner of the DRU. Refer DmaUtilsAutoInc3d_druOwner for valid values
int32_t DmaUtilsAutoInc3d_InitParam::traceLogLevel |
Level for debug messages
int32_t(* DmaUtilsAutoInc3d_InitParam::DmaUtilsVprintf) (const char *format, va_list arg) |
Call back Function pointer to Write Log
Udma_DrvHandle DmaUtilsAutoInc3d_InitParam::udmaDrvHandle |
Handle to the UDMA driver to be used for the utility. If user sets it to NULL then utility will use a default udma driver handle