![]() |
PDK API Guide for J721E
|
Capture status structure used to get the current status.
Data Fields | |
uint32_t | queueCount [CSIRX_NUM_CH] |
uint32_t | dequeueCount [CSIRX_NUM_CH] |
uint32_t | dropCount [CSIRX_NUM_CH] |
uint32_t | errorFrameCount [CSIRX_NUM_CH] |
uint32_t | overflowCount |
uint32_t | spuriousUdmaIntrCount |
uint32_t | frontFIFOOvflCount |
uint32_t | crcCount |
uint32_t | eccCount |
uint32_t | correctedEccCount |
uint32_t | dataIdErrorCount |
uint32_t | invalidAccessCount |
uint32_t | invalidSpCount |
uint32_t | strmFIFOOvflCount [CSIRX_NUM_STREAM] |
uint32_t Csirx_InstStatus::queueCount[CSIRX_NUM_CH] |
Counter to keep track of how many requests are queued to the driver. Note: This counter will be reset at the time of driver init.
uint32_t Csirx_InstStatus::dequeueCount[CSIRX_NUM_CH] |
Counter to keep track of how many requests are dequeued from the driver. Note: This counter will be reset at the time of driver init.
uint32_t Csirx_InstStatus::dropCount[CSIRX_NUM_CH] |
Counter to keep track of how many frames are dropped from the driver when no buffers are queued by the application. Note: This counter will be reset at the time of driver init.
uint32_t Csirx_InstStatus::errorFrameCount[CSIRX_NUM_CH] |
Counter to keep track number of error or incomplete frames from the driver. Note: This counter will be reset at the time of driver init.
uint32_t Csirx_InstStatus::overflowCount |
Counter to keep track of the occurrence of overflow error. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::spuriousUdmaIntrCount |
Counter to keep track of the occurrences of spurious UDMA interrupts. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::frontFIFOOvflCount |
Counter to keep track of the occurrences of Front FIFO Overflow. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::crcCount |
Counter to keep track of the occurrences of CRC errors. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::eccCount |
Counter to keep track of the occurrences of un-corrected ECC errors. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::correctedEccCount |
Counter to keep track of the occurrences of corrected ECC errors. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::dataIdErrorCount |
Counter to keep track of the occurrences of Data ID errors. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::invalidAccessCount |
Counter to keep track of the occurrences of Invalid accesses. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::invalidSpCount |
Counter to keep track of the occurrences of reception of invalid short packet. Note: This counter will be reset at the time of driver create and during driver start.
uint32_t Csirx_InstStatus::strmFIFOOvflCount[CSIRX_NUM_STREAM] |
Counter to keep track of the occurrences of Front FIFO Overflow. Note: This counter will be reset at the time of driver create and during driver start.