![]() |
PDK API Guide for J721E
|
CPSW 5G or 9G MAC port statistics.
Statistics values reported by the CPSW hardware for the Ethernet MAC port.
uint64_t CpswStats_MacPort_Ng::rxGoodFrames |
Total number of good frames received
uint64_t CpswStats_MacPort_Ng::rxBcastFrames |
Total number of good multicast frames received
uint64_t CpswStats_MacPort_Ng::rxMcastFrames |
Total number of good multicast frames received
uint64_t CpswStats_MacPort_Ng::rxPauseFrames |
Total number of pause frames received
uint64_t CpswStats_MacPort_Ng::rxCrcErrors |
Total number of CRC error frames received
uint64_t CpswStats_MacPort_Ng::rxAlignCodeErrors |
Total number of alignment/code errors received
uint64_t CpswStats_MacPort_Ng::rxOversizedFrames |
Total number of oversized frames received
uint64_t CpswStats_MacPort_Ng::rxJabberFrames |
Total number of jabber frames received
uint64_t CpswStats_MacPort_Ng::rxUndersizedFrames |
Total number of undersized frames received
uint64_t CpswStats_MacPort_Ng::rxFragments |
Total number of fragmented frames received
uint64_t CpswStats_MacPort_Ng::aleDrop |
Total number of frames dropped by the ALE
uint64_t CpswStats_MacPort_Ng::aleOverrunDrop |
Total number of overrun frames dropped by the ALE
uint64_t CpswStats_MacPort_Ng::rxOctets |
Total number of received bytes in good frames
uint64_t CpswStats_MacPort_Ng::txGoodFrames |
Total number of good frames transmitted
uint64_t CpswStats_MacPort_Ng::txBcastFrames |
Total number of good broadcast frames transmitted
uint64_t CpswStats_MacPort_Ng::txMcastFrames |
Total number of good multicast frames transmitted
uint64_t CpswStats_MacPort_Ng::txPauseFrames |
Total number of pause frames transmitted
uint64_t CpswStats_MacPort_Ng::txDeferredFrames |
Total number of deferred frames transmitted
uint64_t CpswStats_MacPort_Ng::txCollisionFrames |
Total number of transmitted frames experiencing a collsion
uint64_t CpswStats_MacPort_Ng::txSingleCollFrames |
Total number of transmitted frames experiencing a single collision
uint64_t CpswStats_MacPort_Ng::txMultipleCollFrames |
Total number of transmitted frames experiencing multiple collisions
uint64_t CpswStats_MacPort_Ng::txExcessiveCollFrames |
Total number of transmitted frames abandoned due to excessive collisions
uint64_t CpswStats_MacPort_Ng::txLateCollFrames |
Total number of transmitted frames abandoned due to a late collision
uint64_t CpswStats_MacPort_Ng::rxIPGError |
Total number of receive inter-packet gap errors (10G only)
uint64_t CpswStats_MacPort_Ng::txCarrierSenseErrors |
Total number of transmitted frames that experienced a carrier loss
uint64_t CpswStats_MacPort_Ng::txOctets |
Total number of bytes in all good frames transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames64 |
Total number of 64-byte frames received and transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames65to127 |
Total number of frames of size 65 to 127 bytes received and transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames128to255 |
Total number of frames of size 128 to 255 bytes received and transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames256to511 |
Total number of frames of size 256 to 511 bytes received and transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames512to1023 |
Total number of frames of size 512 to 1023 bytes received and transmitted
uint64_t CpswStats_MacPort_Ng::octetsFrames1024 |
Total number of frames of size 1024 or greater transmitted
uint64_t CpswStats_MacPort_Ng::netOctets |
Total number of bytes received and transmitted
uint64_t CpswStats_MacPort_Ng::rxBottomOfFifoDrop |
Receive bottom of FIFO drop
uint64_t CpswStats_MacPort_Ng::portMaskDrop |
Total number of dropped frames received due to portmask
uint64_t CpswStats_MacPort_Ng::rxTopOfFifoDrop |
Receive top of FIFO drop
uint64_t CpswStats_MacPort_Ng::aleRateLimitDrop |
Total number of frames dropped due to ALE rate limiting
uint64_t CpswStats_MacPort_Ng::aleVidIngressDrop |
Total number of dropped frames due to ALE VID ingress
uint64_t CpswStats_MacPort_Ng::aleDAEqSADrop |
Total number of dropped frames due to DA = SA
uint64_t CpswStats_MacPort_Ng::aleBlockDrop |
Total number of dropped frames due to ALE block mode
uint64_t CpswStats_MacPort_Ng::aleSecureDrop |
Total number of dropped frames due to ALE secure mode
uint64_t CpswStats_MacPort_Ng::aleAuthDrop |
Total number of dropped frames due to ALE authentication
uint64_t CpswStats_MacPort_Ng::aleUnknownUcast |
ALE receive unknown unicast
uint64_t CpswStats_MacPort_Ng::aleUnknownUcastBcnt |
ALE receive unknown unicast bytecount
uint64_t CpswStats_MacPort_Ng::aleUnknownMcast |
ALE receive unknown multicast
uint64_t CpswStats_MacPort_Ng::aleUnknownMcastBcnt |
ALE receive unknown multicast bytecount
uint64_t CpswStats_MacPort_Ng::aleUnknownBcast |
ALE receive unknown broadcast
uint64_t CpswStats_MacPort_Ng::aleUnknownBcastBcnt |
ALE receive unknown broadcast bytecount
uint64_t CpswStats_MacPort_Ng::alePolicyMatch |
ALE policer matched
uint64_t CpswStats_MacPort_Ng::alePolicyMatchRed |
ALE policer matched and condition red
uint64_t CpswStats_MacPort_Ng::alePolicyMatchYellow |
ALE policer matched and condition yellow
uint64_t CpswStats_MacPort_Ng::aleMultSADrop |
ALE multicast source address drop
uint64_t CpswStats_MacPort_Ng::aleDualVlanDrop |
ALE dual VLAN drop
uint64_t CpswStats_MacPort_Ng::aleLenErrorDrop |
ALE IEEE 802.3 length error drop
uint64_t CpswStats_MacPort_Ng::aleIpNextHdrDrop |
ALE IP next header limit drop
uint64_t CpswStats_MacPort_Ng::aleIPv4FragDrop |
ALE IPv4 fragment drop
uint64_t CpswStats_MacPort_Ng::reserved57to80[24U] |
Reserved
uint64_t CpswStats_MacPort_Ng::ietRxAssemblyErr |
IET receive assembly error
uint64_t CpswStats_MacPort_Ng::ietRxAssemblyOk |
IET receive assembly OK
uint64_t CpswStats_MacPort_Ng::ietRxSmdError |
IET receive SMD error
uint64_t CpswStats_MacPort_Ng::ietRxFrag |
IET recieve merge fragment count
uint64_t CpswStats_MacPort_Ng::ietTxHold |
IET transmit merge fragment count
uint64_t CpswStats_MacPort_Ng::ietTxFrag |
IET transmit merge hold count
uint64_t CpswStats_MacPort_Ng::reserved87to95[9U] |
Reserved
uint64_t CpswStats_MacPort_Ng::txMemProtectError |
Transmit memory protect CRC error
uint64_t CpswStats_MacPort_Ng::txPri[8U] |
Ethernet port priority packet count
uint64_t CpswStats_MacPort_Ng::txPriBcnt[8U] |
Ethernet port priority packet byet count
uint64_t CpswStats_MacPort_Ng::txPriDrop[8U] |
Ethernet port priority packet drop count
uint64_t CpswStats_MacPort_Ng::txPriDropBcnt[8U] |
Ethernet port priority packet drop byte count