![]() |
PDK API Guide for J721E
|
MAC port module configuration parameters.
This is the MAC port configuration type expected to be passed to the EnetMod_open() function, as it includes no only the MAC port specific configuration but also the configuration parameters shared with PHY, such as MII interface type and link configuration.
Data Fields | |
CpswMacPort_Cfg | macCfg |
EnetMacPort_Interface | mii |
EnetMacPort_LinkCfg | linkCfg |
CpswMacPort_Cfg CpswMacPort_ModCfg::macCfg |
MAC port specific configuration
EnetMacPort_Interface CpswMacPort_ModCfg::mii |
MAC port MII interface
EnetMacPort_LinkCfg CpswMacPort_ModCfg::linkCfg |
Link configuration (speed and duplexity)