![]() |
PDK API Guide for J721E
|
CSL_UdmapTR4 specifies a Type 4 (Four dimensional data move with data formatting) Transfer Request.
Data Fields | |
uint32_t | flags |
uint16_t | icnt0 |
uint16_t | icnt1 |
uint64_t | addr |
int32_t | dim1 |
uint16_t | icnt2 |
uint16_t | icnt3 |
int32_t | dim2 |
int32_t | dim3 |
uint32_t | fmtflags |
uint32_t CSL_UdmapTR4::flags |
Specifies type of TR and how the TR should be handled. It also supports the TR triggering and output events.
uint16_t CSL_UdmapTR4::icnt0 |
Total loop iteration count for level 0 (innermost)
uint16_t CSL_UdmapTR4::icnt1 |
Total loop iteration count for level 1
uint64_t CSL_UdmapTR4::addr |
Starting address for the source data or destination data if it is a half duplex write
int32_t CSL_UdmapTR4::dim1 |
Signed dimension for loop level 1 for the source data
uint16_t CSL_UdmapTR4::icnt2 |
Total loop iteration count for level 2
uint16_t CSL_UdmapTR4::icnt3 |
Total loop iteration count for level 3 (outermost)
int32_t CSL_UdmapTR4::dim2 |
Signed dimension for loop level 2
int32_t CSL_UdmapTR4::dim3 |
Signed dimension for loop level 3
uint32_t CSL_UdmapTR4::fmtflags |
Tells how the data is formatted either between the input and the output or if the data should use different addressing schemes or sizes