![]() |
PDK API Guide for J721E
|
LCD Configuration for Time Division Multiplexing.
Data Fields | |
uint32_t | tdmEnable |
uint32_t | tdmUnusedBitsLevel |
uint32_t | tdmCycleFormat |
uint32_t | tdmParallelMode |
uint32_t | numBitsPixel1Cycle0 |
uint32_t | numBitsPixel1Cycle1 |
uint32_t | numBitsPixel1Cycle2 |
uint32_t | bitAlignPixel1Cycle0 |
uint32_t | bitAlignPixel1Cycle1 |
uint32_t | bitAlignPixel1Cycle2 |
uint32_t | numBitsPixel2Cycle0 |
uint32_t | numBitsPixel2Cycle1 |
uint32_t | numBitsPixel2Cycle2 |
uint32_t | bitAlignPixel2Cycle0 |
uint32_t | bitAlignPixel2Cycle1 |
uint32_t | bitAlignPixel2Cycle2 |
uint32_t CSL_DssVpLcdTdmCfg::tdmEnable |
Enable the multiple cycle format for the VP output FALSE: Disable TDM TRUE: Enable TDM
uint32_t CSL_DssVpLcdTdmCfg::tdmUnusedBitsLevel |
State of unused bits (TDM mode only) for the VP output. For valid values see CSL_DssVpTdmUnusedBitsLevel
uint32_t CSL_DssVpLcdTdmCfg::tdmCycleFormat |
Cycle format (TDM mode only) for the VP output. For valid values see CSL_DssVpTdmCycleFormat
uint32_t CSL_DssVpLcdTdmCfg::tdmParallelMode |
Output interface width (TDM mode only) for the VP output. For valid values see CSL_DssVpTdmParallelMode
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel1Cycle0 |
Number of bits from the pixel 1 for cycle 0(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel1Cycle1 |
Number of bits from the pixel 1 for cycle 1(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel1Cycle2 |
Number of bits from the pixel 1 for cycle 2(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel1Cycle0 |
Alignment of the bits from pixel 1 for cycle0 on the output interface
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel1Cycle1 |
Alignment of the bits from pixel 1 for cycle1 on the output interface
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel1Cycle2 |
Alignment of the bits from pixel 1 for cycle2 on the output interface
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel2Cycle0 |
Number of bits from the pixel 2 for cycle 0(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel2Cycle1 |
Number of bits from the pixel 2 for cycle 1(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::numBitsPixel2Cycle2 |
Number of bits from the pixel 2 for cycle 2(value from 0 to 16 bits). The values from 17 to 31 are invalid
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel2Cycle0 |
Alignment of the bits from pixel 2 for cycle 0 on the output interface
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel2Cycle1 |
Alignment of the bits from pixel 2 for cycle 1 on the output interface
uint32_t CSL_DssVpLcdTdmCfg::bitAlignPixel2Cycle2 |
Alignment of the bits from pixel 2 for cycle 2 on the output interface