![]() |
PDK API Guide for J721E
|
This structure contains the parameters to setup a event.
Data Fields | |
uint32_t | secureClaimEnable |
uint32_t | evtSendEnable |
uint32_t | rtMap |
uint32_t | extEvtNum |
uint32_t | c7xEvtNum |
uint32_t CSL_ClecEventConfig::secureClaimEnable |
[IN] TRUE/FALSE. When set to TRUE, a non-secure read/write to MRR will generate a privilege error.
uint32_t CSL_ClecEventConfig::evtSendEnable |
[IN] TRUE/FALSE. Controls whether ESR sends this event when written. When set to TRUE, write to ESR triggers the event.
uint32_t CSL_ClecEventConfig::rtMap |
[IN] Route map bit field. Refer CSL_ClecRouteMap.
uint32_t CSL_ClecEventConfig::extEvtNum |
[IN] Encoded external event number to send when this event is triggered. Range 0 to (CSL_CLEC_MAX_EXT_EVT_OUT - 1).
uint32_t CSL_ClecEventConfig::c7xEvtNum |
[IN] C7x event number to send when this event is triggered. Range 0 to (CSL_CLEC_MAX_C7X_EVT_OUT - 1).