PDK API Guide for J721E
|
CPSW_THRU_RATE register.
Holds CPSW_THRU_RATE register contents.
Data Fields | |
Uint32 | enetRxThruRate |
Uint32 | cppiRxThruRate |
Uint32 CSL_CPSW_THRURATE::enetRxThruRate |
Ethernet Port Switch FIFO receive through rate. This register value is the maximum throughput of the Ethernet ports to the crossbar SCR. The default is one 8-byte word for every 3 VBUSP_GCLK periods maximum. The minimum value is 2. This is not a field that is intended to be changed by a user
Uint32 CSL_CPSW_THRURATE::cppiRxThruRate |
CPPI FIFO (port 0) receive through rate. This register value is the maximum throughput of the CPPI FIFO (port 0) into the CPSW_NU. The minimum value is 1. This field is not intended to be changed by the user