![]() |
PDK API Guide for J721E
|
Holds CPPI_P0_FIFO_Status register contents. This is not applicable for 2 port switch.
Data Fields | |
Uint32 | p0TxPriActivePri0 |
Uint32 | p0TxPriActivePri1 |
Uint32 | p0TxPriActivePri2 |
Uint32 | p0TxPriActivePri3 |
Uint32 | p0TxPriActivePri4 |
Uint32 | p0TxPriActivePri5 |
Uint32 | p0TxPriActivePri6 |
Uint32 | p0TxPriActivePri7 |
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri0 |
Port 0 Transmit FIFO Priority Active for priority 0 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri1 |
Port 0 Transmit FIFO Priority Active for priority 1 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri2 |
Port 0 Transmit FIFO Priority Active for priority 2 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri3 |
Port 0 Transmit FIFO Priority Active for priority 3 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri4 |
Port 0 Transmit FIFO Priority Active for priority 4 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri5 |
Port 0 Transmit FIFO Priority Active for priority 5 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri6 |
Port 0 Transmit FIFO Priority Active for priority 6 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).
Uint32 CSL_CPSW_CPPI_P0_FIFOSTATUS::p0TxPriActivePri7 |
Port 0 Transmit FIFO Priority Active for priority 7 Indicates whether the corresponding FIFO priority has one or more queued packets on it or not. note: for N=2 this field is always zero (there is no transmit FIFO).